Defines command to be executed using STIG mechanism.

Public Attributes#

uint8_t

Command op-code.

uint16_t

Number of Read Data Bytes.

uint8_t

Number of Address Bytes.

uint8_t

Number of Write Data Bytes.

uint8_t

Number of dummy cycles.

bool

Mode Bit Configuration register are sent following the address bytes.

uint32_t

Flash command address.

void *

Buffer for read data.

void *

Buffer with data to write.

Public Attribute Documentation#

cmdOpcode#

uint8_t QSPI_StigCmd_TypeDef::cmdOpcode

Command op-code.


readDataSize#

uint16_t QSPI_StigCmd_TypeDef::readDataSize

Number of Read Data Bytes.


addrSize#

uint8_t QSPI_StigCmd_TypeDef::addrSize

Number of Address Bytes.


writeDataSize#

uint8_t QSPI_StigCmd_TypeDef::writeDataSize

Number of Write Data Bytes.


dummyCycles#

uint8_t QSPI_StigCmd_TypeDef::dummyCycles

Number of dummy cycles.


modeBitEnable#

bool QSPI_StigCmd_TypeDef::modeBitEnable

Mode Bit Configuration register are sent following the address bytes.


address#

uint32_t QSPI_StigCmd_TypeDef::address

Flash command address.


readBuffer#

void* QSPI_StigCmd_TypeDef::readBuffer

Buffer for read data.


writeBuffer#

void* QSPI_StigCmd_TypeDef::writeBuffer

Buffer with data to write.