A Cycle Counter Instance.

Public Attributes#

uint32_t

Cycle counter at start of recording.

uint32_t

Cycles elapsed in last recording.

uint32_t

Max recorded cycles since last reset or init.

Public Attribute Documentation#

start#

uint32_t dwt_cycle_counter_handle_t::start

Cycle counter at start of recording.


Definition at line 281 of file platform/emlib/src/em_core.c

cycles#

uint32_t dwt_cycle_counter_handle_t::cycles

Cycles elapsed in last recording.


Definition at line 282 of file platform/emlib/src/em_core.c

max#

uint32_t dwt_cycle_counter_handle_t::max

Max recorded cycles since last reset or init.


Definition at line 283 of file platform/emlib/src/em_core.c