Tamper Response#

In CPMS, the default tamper configuration is automatically displayed for Secure Vault High (SVH) HSE and Series 3 Secure Vault devices. These configurations can be customized only for Secure Vault High and Series 3 Secure Vault devices.

Anti-tamper protection is available only on Secure Vault High and Series 3 Secure Vault devices. Each tamper configuration can be assigned one of five tamper response levels, ranging from ignoring the tamper event to erasing the device OTP.

When tamper protection is configured on a Secure Vault High or Series 3 Secure Vault device, CPMS requires a public command key.

For more information about anti-tamper protection, see Anti-Tamper Protection Configuration and Use.

For Series 2 devices, configure tamper settings in the CPMS portal as shown in the following figure.

screenshotscreenshot

For Series 3 devices, configure tamper settings in the CPMS portal or optionally upload a configuration.json file, as shown in the following figure.

CPMS Configure Secure Boot screenshotCPMS Configure Secure Boot screenshot