cdc.h File Reference
USB Communication Device Class (CDC) driver.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        cdc.h
       
       .
      
| Functions | |
| void | CDC_Init (void) | 
| CDC device initialization. | |
| int | CDC_SetupCmd (const USB_Setup_TypeDef *setup) | 
| Handle USB setup commands. Implements CDC class specific commands. | |
| void | CDC_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| Callback function called each time the USB device state is changed. Starts CDC operation when device has been configured by USB host. | |