LESENSE_DecStCond_TypeDef Struct ReferenceEMLIB > LESENSE
Decoder state condition descriptor structure.
       Definition at line
       
        1022
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
| Data Fields | |
| uint8_t | compMask | 
| uint8_t | compVal | 
| uint8_t | nextState | 
| LESENSE_StTransAct_TypeDef | prsAct | 
| bool | setInt | 
Field Documentation
| uint8_t LESENSE_DecStCond_TypeDef::compMask | 
Configure compare mask. Set bit X to exclude sensor X from evaluation. Note: decoder can handle sensor inputs from up to 4 sensors, therefore this mask is 4 bit long.
        Definition at line
        
         1030
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_DecoderStateConfig() .
| uint8_t LESENSE_DecStCond_TypeDef::compVal | 
Configure compare value. State transition is triggered when sensor state equals to this value. Valid range: 0-15 (4 bits).
        Definition at line
        
         1025
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_DecoderStateConfig() .
| uint8_t LESENSE_DecStCond_TypeDef::nextState | 
Configure index of state to be entered if the sensor state equals to compVal. Valid range: 0-15 (4 bits).
        Definition at line
        
         1034
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_DecoderStateConfig() .
| LESENSE_StTransAct_TypeDef LESENSE_DecStCond_TypeDef::prsAct | 
Configure which PRS action to perform when sensor state equals to compVal.
        Definition at line
        
         1038
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_DecoderStateConfig() .
| bool LESENSE_DecStCond_TypeDef::setInt | 
If enabled, interrupt flag is set when sensor state equals to compVal.
        Definition at line
        
         1041
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_DecoderStateConfig() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_lesense.h