LETIMER_Init_TypeDef Struct ReferenceEMLIB > LETIMER
LETIMER initialization structure.
Definition at line 93
of file em_letimer.h
.
#include <
em_letimer.h
>
Data Fields | |
bool | bufTop |
bool | comp0Top |
bool | debugRun |
bool | enable |
uint8_t | out0Pol |
uint8_t | out1Pol |
LETIMER_RepeatMode_TypeDef | repMode |
LETIMER_UFOA_TypeDef | ufoa0 |
LETIMER_UFOA_TypeDef | ufoa1 |
Field Documentation
bool LETIMER_Init_TypeDef::bufTop |
Load COMP1 into COMP0 when REP0 reaches 0.
Definition at line 101
of file em_letimer.h
.
Referenced by LETIMER_Init().
bool LETIMER_Init_TypeDef::comp0Top |
Load COMP0 register into CNT when counter underflows.
Definition at line 100
of file em_letimer.h
.
Referenced by LETIMER_Init(), and MIC_init().
bool LETIMER_Init_TypeDef::debugRun |
Counter shall keep running during debug halt.
Definition at line 95
of file em_letimer.h
.
Referenced by LETIMER_Init().
bool LETIMER_Init_TypeDef::enable |
Start counting when init completed.
Definition at line 94
of file em_letimer.h
.
Referenced by LETIMER_Init(), and MIC_init().
uint8_t LETIMER_Init_TypeDef::out0Pol |
uint8_t LETIMER_Init_TypeDef::out1Pol |
LETIMER_RepeatMode_TypeDef LETIMER_Init_TypeDef::repMode |
LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa0 |
Underflow output 0 action.
Definition at line 104
of file em_letimer.h
.
Referenced by LETIMER_Init(), and MIC_init().
LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa1 |
Underflow output 1 action.
Definition at line 105
of file em_letimer.h
.
Referenced by LETIMER_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_letimer.h