UARTDRV_Buffer_FifoQueue_t Struct ReferenceEMDRV > UARTDRV
Transfer operation FIFO queue typedef.
       Definition at line
       
        138
       
       of file
       
        uartdrv.h
       
       .
      
      
       #include <
       
     
        uartdrv.h
       
       >
      
| Data Fields | |
| UARTDRV_Buffer_t | fifo [] | 
| FIFO of queued data. | |
| volatile uint16_t | head | 
| An index of the next byte to send. | |
| const uint16_t | size | 
| FIFO size. | |
| volatile uint16_t | tail | 
| An index of the location to enqueue the next message. | |
| volatile uint16_t | used | 
| A number of bytes queued. | |
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emdrv/uartdrv/inc/
       uartdrv.h