CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Init values should be obtained from a configuration tool, app note or xtal datasheet
Definition at line
1395
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
bool | autoSelEm01 |
bool | autoStartEm01 |
bool | autoStartSelOnRacWakeup |
uint16_t | ctuneStartup |
uint16_t | ctuneSteadyState |
bool | lowPowerMode |
CMU_OscMode_TypeDef | mode |
uint8_t | regIshSteadyState |
uint8_t | thresholdPeakDetect |
uint8_t | timeoutPeakDetect |
uint8_t | timeoutShuntOptimization |
uint8_t | timeoutStartup |
uint8_t | timeoutSteady |
uint8_t | xoCoreBiasTrimStartup |
uint8_t | xoCoreBiasTrimSteadyState |
Field Documentation
bool CMU_HFXOInit_TypeDef::autoSelEm01 |
- Deprecated:
- Use CMU_HFXOAutostartEnable instead.
Definition at line
1407
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
bool CMU_HFXOInit_TypeDef::autoStartEm01 |
- Deprecated:
- Use CMU_HFXOAutostartEnable instead.
Definition at line
1406
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup |
- Deprecated:
- Use CMU_HFXOAutostartEnable instead.
Definition at line
1408
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
uint16_t CMU_HFXOInit_TypeDef::ctuneStartup |
Startup phase CTUNE (load capacitance) value
Definition at line
1409
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState |
Steady-state phase CTUNE (load capacitance) value
Definition at line
1410
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
bool CMU_HFXOInit_TypeDef::lowPowerMode |
CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState |
Shunt steady-state current
Definition at line
1411
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect |
uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect |
uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization |
Timeout - shunt optimization
Definition at line
1415
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
uint8_t CMU_HFXOInit_TypeDef::timeoutStartup |
uint8_t CMU_HFXOInit_TypeDef::timeoutSteady |
uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup |
Startup XO core bias current trim
Definition at line
1412
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState |
Steady-state XO core bias current trim
Definition at line
1413
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_cmu.h