UARTDRV_InitLeuart_t Struct ReferenceEMDRV > UARTDRV

LEUART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required to initialize a driver instance. This structure is passed to UARTDRV_InitLeuart() when initializing a UARTDRV instance.

Definition at line 208 of file uartdrv.h.

#include <uartdrv.h>

Data Fields

uint32_t baudRate
 UART baud rate.
 
uint8_t ctsPin
 CTS pin number.
 
GPIO_Port_TypeDef ctsPort
 CTS pin port number.
 
UARTDRV_FlowControlType_t fcType
 Flow control mode.
 
LEUART_Parity_TypeDef parity
 Parity configuration.
 
LEUART_TypeDefport
 The peripheral used for LEUART.
 
uint8_t portLocationRx
 Location number for LEUART Rx pin.
 
uint8_t portLocationTx
 Location number for LEUART Tx pin.
 
uint8_t rtsPin
 RTS pin number.
 
GPIO_Port_TypeDef rtsPort
 RTS pin port number.
 
UARTDRV_Buffer_FifoQueue_trxQueue
 Receive operation queue.
 
LEUART_Stopbits_TypeDef stopBits
 Number of stop bits.
 
UARTDRV_Buffer_FifoQueue_ttxQueue
 Transmit operation queue.
 

The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emdrv/uartdrv/inc/uartdrv.h