tftamapped.c File Reference

EFM32GG_DK3750, TFT Initialization and setup for Adress Mapped mode.

Version
5.4.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file tftamapped.c.

#include <stdbool.h>
#include "em_device.h"
#include "em_gpio.h"
#include "em_ebi.h"
#include "bsp.h"
#include "tftamapped.h"
#include "dmd/ssd2119/dmd_ssd2119.h"
#include "glib/glib.h"

Functions

bool TFT_AddressMappedInit (void)
 TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
 

Variables

static bool runOnce = true
 

Variable Documentation

bool runOnce = true
static

Flag to indicate that we need to initialize once if starting up in

Definition at line 27 of file tftamapped.c.

Referenced by TFT_AddressMappedInit().