LESENSE_DecCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE decoder control descriptor structure.
Definition at line 671
of file em_lesense.h
.
#include <
em_lesense.h
>
Data Fields | |
bool | chkState |
LESENSE_DecInput_TypeDef | decInput |
bool | hystIRQ |
bool | hystPRS0 |
bool | hystPRS1 |
bool | hystPRS2 |
uint32_t | initState |
bool | intMap |
LESENSE_PRSSel_TypeDef | prsChSel0 |
LESENSE_PRSSel_TypeDef | prsChSel1 |
LESENSE_PRSSel_TypeDef | prsChSel2 |
LESENSE_PRSSel_TypeDef | prsChSel3 |
bool | prsCount |
Field Documentation
bool LESENSE_DecCtrlDesc_TypeDef::chkState |
Set to enable the decoder to check the present state in addition to the states defined in TCONF.
Definition at line 680
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput |
Select the input to the LESENSE decoder.
Definition at line 673
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ |
Set to enable hysteresis in the decoder for suppressing interrupt requests.
Definition at line 700
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0 |
Set to enable hysteresis in the decoder for suppressing changes on PRS channel 0.
Definition at line 688
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1 |
Set to enable hysteresis in the decoder for suppressing changes on PRS channel 1.
Definition at line 692
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2 |
Set to enable hysteresis in the decoder for suppressing changes on PRS channel 2.
Definition at line 696
of file em_lesense.h
.
Referenced by LESENSE_Init().
uint32_t LESENSE_DecCtrlDesc_TypeDef::initState |
Initial state of the LESENSE decoder.
Definition at line 676
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_DecCtrlDesc_TypeDef::intMap |
When set, a transition from state x in the decoder will set interrupt flag CHx.
Definition at line 684
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0 |
Select PRS channel input for bit 0 of the LESENSE decoder.
Definition at line 707
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1 |
Select PRS channel input for bit 1 of the LESENSE decoder.
Definition at line 710
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2 |
Select PRS channel input for bit 2 of the LESENSE decoder.
Definition at line 713
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3 |
Select PRS channel input for bit 3 of the LESENSE decoder.
Definition at line 716
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_DecCtrlDesc_TypeDef::prsCount |
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.
Definition at line 704
of file em_lesense.h
.
Referenced by LESENSE_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h