LETIMER_TypeDef Struct ReferenceDevices > LETIMER
LETIMER Register Declaration
Definition at line 49
of file efr32fg14p_letimer.h
.
#include <
efr32fg14p_letimer.h
>
Data Fields | |
__IOM uint32_t | CMD |
__IOM uint32_t | CNT |
__IOM uint32_t | COMP0 |
__IOM uint32_t | COMP1 |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | PRSSEL |
__IOM uint32_t | REP0 |
__IOM uint32_t | REP1 |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [2] |
uint32_t | RESERVED2 [2] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTEPEN |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t LETIMER_TypeDef::CMD |
Command Register
Definition at line 51
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_Enable(), LETIMER_Init(), and LETIMER_Reset().
__IOM uint32_t LETIMER_TypeDef::CNT |
Counter Value Register
Definition at line 53
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_CounterGet().
__IOM uint32_t LETIMER_TypeDef::COMP0 |
Compare Value Register 0
Definition at line 54
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_CompareGet(), LETIMER_CompareSet(), and LETIMER_Reset().
__IOM uint32_t LETIMER_TypeDef::COMP1 |
Compare Value Register 1
Definition at line 55
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_CompareGet(), LETIMER_CompareSet(), and LETIMER_Reset().
__IOM uint32_t LETIMER_TypeDef::CTRL |
Control Register
Definition at line 50
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_Init(), and LETIMER_Reset().
__IOM uint32_t LETIMER_TypeDef::IEN |
Interrupt Enable Register
Definition at line 61
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_IntDisable(), LETIMER_IntEnable(), LETIMER_IntGetEnabled(), and LETIMER_Reset().
__IM uint32_t LETIMER_TypeDef::IF |
Interrupt Flag Register
Definition at line 58
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_IntGet(), and LETIMER_IntGetEnabled().
__IOM uint32_t LETIMER_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 60
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_IntClear(), and LETIMER_Reset().
__IOM uint32_t LETIMER_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 59
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_IntSet().
__IOM uint32_t LETIMER_TypeDef::PRSSEL |
PRS Input Select Register
Definition at line 71
of file efr32fg14p_letimer.h
.
__IOM uint32_t LETIMER_TypeDef::REP0 |
Repeat Counter Register 0
Definition at line 56
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_RepeatGet(), LETIMER_RepeatSet(), and LETIMER_Reset().
__IOM uint32_t LETIMER_TypeDef::REP1 |
Repeat Counter Register 1
Definition at line 57
of file efr32fg14p_letimer.h
.
Referenced by LETIMER_RepeatGet(), LETIMER_RepeatSet(), and LETIMER_Reset().
uint32_t LETIMER_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 63
of file efr32fg14p_letimer.h
.
uint32_t LETIMER_TypeDef::RESERVED1[2] |
Reserved for future use
Definition at line 66
of file efr32fg14p_letimer.h
.
uint32_t LETIMER_TypeDef::RESERVED2[2] |
Reserved for future use
Definition at line 70
of file efr32fg14p_letimer.h
.
__IOM uint32_t LETIMER_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 68
of file efr32fg14p_letimer.h
.
__IOM uint32_t LETIMER_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line 67
of file efr32fg14p_letimer.h
.
__IM uint32_t LETIMER_TypeDef::STATUS |
__IM uint32_t LETIMER_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 64
of file efr32fg14p_letimer.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG14P/Include/
efr32fg14p_letimer.h