SMU_TypeDef Struct ReferenceDevices > SMU

SMU Register Declaration

Definition at line 49 of file efr32fg14p_smu.h.

#include <efr32fg14p_smu.h>

Data Fields

__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t PPUCTRL
 
__IM uint32_t PPUFS
 
__IOM uint32_t PPUPATD0
 
__IOM uint32_t PPUPATD1
 
uint32_t RESERVED0 [3]
 
uint32_t RESERVED1 [9]
 
uint32_t RESERVED2 [3]
 
uint32_t RESERVED3 [14]
 

Field Documentation

__IOM uint32_t SMU_TypeDef::IEN

Interrupt Enable Register

Definition at line 54 of file efr32fg14p_smu.h.

__IM uint32_t SMU_TypeDef::IF

Interrupt Flag Register

Definition at line 51 of file efr32fg14p_smu.h.

__IOM uint32_t SMU_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 53 of file efr32fg14p_smu.h.

__IOM uint32_t SMU_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 52 of file efr32fg14p_smu.h.

__IOM uint32_t SMU_TypeDef::PPUCTRL

PPU Control Register

Definition at line 57 of file efr32fg14p_smu.h.

__IM uint32_t SMU_TypeDef::PPUFS

PPU Fault Status

Definition at line 63 of file efr32fg14p_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD0

PPU Privilege Access Type Descriptor 0

Definition at line 59 of file efr32fg14p_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD1

PPU Privilege Access Type Descriptor 1

Definition at line 60 of file efr32fg14p_smu.h.

uint32_t SMU_TypeDef::RESERVED0[3]

Reserved for future use

Definition at line 50 of file efr32fg14p_smu.h.

uint32_t SMU_TypeDef::RESERVED1[9]

Reserved for future use

Definition at line 56 of file efr32fg14p_smu.h.

uint32_t SMU_TypeDef::RESERVED2[3]

Reserved for future use

Definition at line 58 of file efr32fg14p_smu.h.

uint32_t SMU_TypeDef::RESERVED3[14]

Reserved for future use

Definition at line 62 of file efr32fg14p_smu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG14P/Include/efr32fg14p_smu.h