LCDEMLIB
Detailed Description
Liquid Crystal Display (LCD) Peripheral API.
This module contains functions to control the LDC peripheral of Silicon Labs 32-bit MCUs and SoCs. The LCD driver can drive up to 8x36 segmented LCD directly. The animation feature makes it possible to have active animations without the CPU intervention.
Data Structures | |
struct | LCD_AnimInit_TypeDef |
struct | LCD_FrameCountInit_TypeDef |
struct | LCD_Init_TypeDef |
Macros | |
#define | LCD_DEFAULT_CONTRAST 15 |
#define | LCD_DEFAULT_FRAME_RATE_DIV 4 |
#define | LCD_INIT_DEFAULT |
Enumerations | |
enum | LCD_AnimLogic_TypeDef { lcdAnimLogicAnd = LCD_BACTRL_ALOGSEL_AND, lcdAnimLogicOr = LCD_BACTRL_ALOGSEL_OR } |
enum | LCD_AnimShift_TypeDef { lcdAnimShiftNone = _LCD_BACTRL_AREGASC_NOSHIFT, lcdAnimShiftLeft = _LCD_BACTRL_AREGASC_SHIFTLEFT, lcdAnimShiftRight = _LCD_BACTRL_AREGASC_SHIFTRIGHT } |
enum | LCD_Bias_TypeDef { lcdBiasStatic = LCD_DISPCTRL_BIAS_STATIC, lcdBiasOneHalf = LCD_DISPCTRL_BIAS_ONEHALF, lcdBiasOneThird = LCD_DISPCTRL_BIAS_ONETHIRD } |
enum | LCD_ConConf_TypeDef { lcdConConfVLCD = LCD_DISPCTRL_CONCONF_VLCD, lcdConConfGND = LCD_DISPCTRL_CONCONF_GND } |
enum | LCD_FCPreScale_TypeDef { lcdFCPrescDiv1 = LCD_BACTRL_FCPRESC_DIV1, lcdFCPrescDiv2 = LCD_BACTRL_FCPRESC_DIV2, lcdFCPrescDiv4 = LCD_BACTRL_FCPRESC_DIV4, lcdFCPrescDiv8 = LCD_BACTRL_FCPRESC_DIV8 } |
enum | LCD_Mux_TypeDef { lcdMuxStatic = LCD_DISPCTRL_MUX_STATIC, lcdMuxDuplex = LCD_DISPCTRL_MUX_DUPLEX, lcdMuxTriplex = LCD_DISPCTRL_MUX_TRIPLEX, lcdMuxQuadruplex = LCD_DISPCTRL_MUX_QUADRUPLEX } |
enum | LCD_SegmentRange_TypeDef { lcdSegment0_3 = (1 << 0), lcdSegment4_7 = (1 << 1), lcdSegment8_11 = (1 << 2), lcdSegment12_15 = (1 << 3), lcdSegment16_19 = (1 << 4), lcdSegment20_23 = (1 << 5), lcdSegment24_27 = (1 << 6), lcdSegment28_31 = (1 << 7), lcdSegment32_35 = (1 << 8), lcdSegment36_39 = (1 << 9), lcdSegmentAll = (0x03ff) } |
enum | LCD_UpdateCtrl_TypeDef { lcdUpdateCtrlRegular = LCD_CTRL_UDCTRL_REGULAR, lcdUpdateCtrlFCEvent = LCD_CTRL_UDCTRL_FCEVENT, lcdUpdateCtrlFrameStart = LCD_CTRL_UDCTRL_FRAMESTART } |
enum | LCD_VBoostLevel_TypeDef { lcdVBoostLevel0 = LCD_DISPCTRL_VBLEV_LEVEL0, lcdVBoostLevel1 = LCD_DISPCTRL_VBLEV_LEVEL1, lcdVBoostLevel2 = LCD_DISPCTRL_VBLEV_LEVEL2, lcdVBoostLevel3 = LCD_DISPCTRL_VBLEV_LEVEL3, lcdVBoostLevel4 = LCD_DISPCTRL_VBLEV_LEVEL4, lcdVBoostLevel5 = LCD_DISPCTRL_VBLEV_LEVEL5, lcdVBoostLevel6 = LCD_DISPCTRL_VBLEV_LEVEL6, lcdVBoostLevel7 = LCD_DISPCTRL_VBLEV_LEVEL7 } |
enum | LCD_VLCDSel_TypeDef { lcdVLCDSelVDD = LCD_DISPCTRL_VLCDSEL_VDD, lcdVLCDSelVExtBoost = LCD_DISPCTRL_VLCDSEL_VEXTBOOST } |
enum | LCD_Wave_TypeDef { lcdWaveLowPower = LCD_DISPCTRL_WAVE_LOWPOWER, lcdWaveNormal = LCD_DISPCTRL_WAVE_NORMAL } |
Functions | |
__STATIC_INLINE void | LCD_AnimEnable (bool enable) |
Enables or disables LCD Animation feature. | |
void | LCD_AnimInit (const LCD_AnimInit_TypeDef *animInit) |
Configure the LCD controller Animation feature. | |
__STATIC_INLINE int | LCD_AnimState (void) |
Returns current animation state. | |
void | LCD_BiasSet (LCD_Bias_TypeDef bias) |
Configure the bias level on the LCD panel. | |
__STATIC_INLINE void | LCD_BlankEnable (bool enable) |
Disables all segments, while keeping segment state. | |
__STATIC_INLINE void | LCD_BlinkEnable (bool enable) |
Enables or disables LCD blink. | |
__STATIC_INLINE int | LCD_BlinkState (void) |
Returns current blink state. | |
void | LCD_ContrastSet (int level) |
Configure the contrast level on the LCD panel. | |
__STATIC_INLINE void | LCD_Enable (bool enable) |
Enable or disable LCD controller. | |
__STATIC_INLINE void | LCD_FrameCountEnable (bool enable) |
Enables or disables LCD Frame Control. | |
void | LCD_FrameCountInit (const LCD_FrameCountInit_TypeDef *fcInit) |
Initialize the LCD Frame Counter. | |
__STATIC_INLINE void | LCD_FreezeEnable (bool enable) |
When set, LCD registers will not be updated until cleared. | |
void | LCD_Init (const LCD_Init_TypeDef *lcdInit) |
Initialize the Liquid Crystal Display (LCD) controller. | |
__STATIC_INLINE void | LCD_IntClear (uint32_t flags) |
Clear one or more interrupt flags. | |
__STATIC_INLINE void | LCD_IntDisable (uint32_t flags) |
Disable LCD interrupts. | |
__STATIC_INLINE void | LCD_IntEnable (uint32_t flags) |
Enable LCD interrupts. | |
__STATIC_INLINE uint32_t | LCD_IntGet (void) |
Get pending LCD interrupt flags. | |
__STATIC_INLINE uint32_t | LCD_IntGetEnabled (void) |
Get enabled and pending LCD interrupt flags. | |
__STATIC_INLINE void | LCD_IntSet (uint32_t flags) |
Set one or more pending LCD interrupts from SW. | |
void | LCD_SegmentRangeEnable (LCD_SegmentRange_TypeDef segmentRange, bool enable) |
Enables updating this range of LCD segment lines. | |
void | LCD_SegmentSet (int com, int bit, bool enable) |
Turn on or clear a segment. | |
void | LCD_SegmentSetHigh (int com, uint32_t mask, uint32_t bits) |
Update the high (32-39) segments on a given COM-line in one operation. | |
void | LCD_SegmentSetLow (int com, uint32_t mask, uint32_t bits) |
Update 0-31 lowest segments on a given COM-line in one operation according to the bit mask. | |
__STATIC_INLINE void | LCD_SyncBusyDelay (uint32_t flags) |
Polls LCD SYNCBUSY flags, until flag has been cleared. | |
__STATIC_INLINE uint32_t | LCD_SyncBusyGet (void) |
Returns SYNCBUSY bits, indicating which registers have pending updates. | |
void | LCD_UpdateCtrl (LCD_UpdateCtrl_TypeDef ud) |
Configure Update Control. | |
void | LCD_VBoostSet (LCD_VBoostLevel_TypeDef vboost) |
Configure voltage booster. | |
void | LCD_VLCDSelect (LCD_VLCDSel_TypeDef vlcd) |
Select a source for VLCD. | |
Macro Definition Documentation
#define LCD_INIT_DEFAULT |
Default configuration for LCD initialization structure, enables 160 segments.
Definition at line 299
of file em_lcd.h
.
Enumeration Type Documentation
enum LCD_Bias_TypeDef |
enum LCD_ConConf_TypeDef |
enum LCD_Mux_TypeDef |
MUX setting.
Definition at line 68
of file em_lcd.h
.
Segment selection.
Definition at line 169
of file em_lcd.h
.
Voltage Boost Level - Data sheets document setting for each part number.
Definition at line 134
of file em_lcd.h
.
enum LCD_VLCDSel_TypeDef |
enum LCD_Wave_TypeDef |
Function Documentation
__STATIC_INLINE void LCD_AnimEnable | ( | bool | enable | ) |
Enables or disables LCD Animation feature.
- Parameters
-
[in] enable
Boolean true enables animation, false disables animation.
Definition at line 383
of file em_lcd.h
.
References LCD, and LCD_BACTRL_AEN.
Referenced by LCD_AnimInit().
void LCD_AnimInit | ( | const LCD_AnimInit_TypeDef * | animInit | ) |
Configure the LCD controller Animation feature.
- Parameters
-
[in] animInit
A pointer to the LCD Animation initialization structure.
Definition at line 201
of file em_lcd.c
.
References _LCD_BACTRL_ALOGSEL_MASK, _LCD_BACTRL_AREGASC_MASK, _LCD_BACTRL_AREGASC_SHIFT, _LCD_BACTRL_AREGBSC_MASK, _LCD_BACTRL_AREGBSC_SHIFT, LCD_AnimInit_TypeDef::animLogic, LCD_AnimInit_TypeDef::AReg, LCD_AnimInit_TypeDef::AShift, LCD_AnimInit_TypeDef::BReg, LCD_AnimInit_TypeDef::BShift, LCD_AnimInit_TypeDef::enable, LCD, and LCD_AnimEnable().
__STATIC_INLINE int LCD_AnimState | ( | void |
| ) |
Returns current animation state.
- Returns
- Animation state, in range 0-15.
Definition at line 447
of file em_lcd.h
.
References _LCD_STATUS_ASTATE_MASK, _LCD_STATUS_ASTATE_SHIFT, and LCD.
void LCD_BiasSet | ( | LCD_Bias_TypeDef | bias | ) |
Configure the bias level on the LCD panel.
- Parameters
-
[in] bias
The bias level.
Definition at line 617
of file em_lcd.c
.
References _LCD_DISPCTRL_BIAS_MASK, and LCD.
__STATIC_INLINE void LCD_BlankEnable | ( | bool | enable | ) |
Disables all segments, while keeping segment state.
- Parameters
-
[in] enable
Boolean true clears all segments, boolean false restores all segment lines.
Definition at line 415
of file em_lcd.h
.
References LCD, and LCD_BACTRL_BLANK.
__STATIC_INLINE void LCD_BlinkEnable | ( | bool | enable | ) |
Enables or disables LCD blink.
- Parameters
-
[in] enable
Boolean true enables blink, false disables blink.
Definition at line 399
of file em_lcd.h
.
References LCD, and LCD_BACTRL_BLINKEN.
__STATIC_INLINE int LCD_BlinkState | ( | void |
| ) |
Returns current blink state.
- Returns
- Return value is 1 if segments are enabled, 0 if disabled.
Definition at line 459
of file em_lcd.h
.
References _LCD_STATUS_BLINK_MASK, _LCD_STATUS_BLINK_SHIFT, and LCD.
void LCD_ContrastSet | ( | int | level | ) |
Configure the contrast level on the LCD panel.
- Parameters
-
[in] level
The contrast level in range 0-31.
Definition at line 584
of file em_lcd.c
.
References _LCD_DISPCTRL_CONLEV_MASK, _LCD_DISPCTRL_CONLEV_SHIFT, and LCD.
Referenced by LCD_Init().
__STATIC_INLINE void LCD_Enable | ( | bool | enable | ) |
Enable or disable LCD controller.
- Parameters
-
[in] enable
If true, enables LCD controller with current configuration. If false, disables LCD controller. Enable CMU clock for LCD for correct operation.
Definition at line 367
of file em_lcd.h
.
References LCD, and LCD_CTRL_EN.
Referenced by LCD_Init(), and SegmentLCD_Disable().
__STATIC_INLINE void LCD_FrameCountEnable | ( | bool | enable | ) |
Enables or disables LCD Frame Control.
- Parameters
-
[in] enable
Boolean true enables frame counter, false disables frame counter.
Definition at line 431
of file em_lcd.h
.
References LCD, and LCD_BACTRL_FCEN.
Referenced by LCD_FrameCountInit().
void LCD_FrameCountInit | ( | const LCD_FrameCountInit_TypeDef * | fcInit | ) |
Initialize the LCD Frame Counter.
- Parameters
-
[in] fcInit
A pointer to the Frame Counter initialization structure.
Definition at line 173
of file em_lcd.c
.
References _LCD_BACTRL_FCPRESC_MASK, _LCD_BACTRL_FCTOP_MASK, _LCD_BACTRL_FCTOP_SHIFT, LCD_FrameCountInit_TypeDef::enable, LCD, LCD_FrameCountEnable(), LCD_FrameCountInit_TypeDef::prescale, and LCD_FrameCountInit_TypeDef::top.
__STATIC_INLINE void LCD_FreezeEnable | ( | bool | enable | ) |
When set, LCD registers will not be updated until cleared.
- Parameters
-
[in] enable
When enable is true, update is stopped; when false, all registers are updated.
Definition at line 472
of file em_lcd.h
.
References LCD, LCD_FREEZE_REGFREEZE_FREEZE, and LCD_FREEZE_REGFREEZE_UPDATE.
Referenced by SegmentLCD_Number(), SegmentLCD_UnsignedHex(), and SegmentLCD_Write().
void LCD_Init | ( | const LCD_Init_TypeDef * | lcdInit | ) |
Initialize the Liquid Crystal Display (LCD) controller.
Configures the LCD controller. You must enable it afterwards, potentially configuring Frame Control and interrupts first according to requirements.
- Parameters
-
[in] lcdInit
A pointer to the initialization structure which configures the LCD controller.
Definition at line 67
of file em_lcd.c
.
References _LCD_DISPCTRL_BIAS_MASK, _LCD_DISPCTRL_CONCONF_MASK, _LCD_DISPCTRL_MUX_MASK, _LCD_DISPCTRL_VLCDSEL_MASK, _LCD_DISPCTRL_WAVE_MASK, LCD_Init_TypeDef::bias, LCD_Init_TypeDef::contrast, LCD_Init_TypeDef::enable, LCD, LCD_ContrastSet(), LCD_Enable(), LCD_Init_TypeDef::mux, LCD_Init_TypeDef::vlcd, and LCD_Init_TypeDef::wave.
Referenced by SegmentLCD_Init().
__STATIC_INLINE void LCD_IntClear | ( | uint32_t | flags | ) |
Clear one or more interrupt flags.
- Parameters
-
[in] flags
LCD interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for LCD module (LCD_IFS_nnn).
Definition at line 600
of file em_lcd.h
.
References LCD.
__STATIC_INLINE void LCD_IntDisable | ( | uint32_t | flags | ) |
Disable LCD interrupts.
- Parameters
-
[in] flags
LCD interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for LCD module (LCD_IFS_nnn).
Definition at line 586
of file em_lcd.h
.
References LCD.
Referenced by SegmentLCD_Init().
__STATIC_INLINE void LCD_IntEnable | ( | uint32_t | flags | ) |
Enable LCD interrupts.
- Parameters
-
[in] flags
LCD interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for LCD module (LCD_IFS_nnn).
Definition at line 572
of file em_lcd.h
.
References LCD.
__STATIC_INLINE uint32_t LCD_IntGet | ( | void |
| ) |
Get pending LCD interrupt flags.
- Returns
- Pending LCD interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the LCD module (LCD_IFS_nnn).
Definition at line 514
of file em_lcd.h
.
References LCD.
__STATIC_INLINE uint32_t LCD_IntGetEnabled | ( | void |
| ) |
Get enabled and pending LCD interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Event bits are not cleared by the use of this function.
- Returns
- Pending and enabled LCD interrupt sources. Return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in LCD_IEN_nnn register (LCD_IEN_nnn) and
- the bitwise OR combination of valid interrupt flags of LCD module (LCD_IF_nnn).
Definition at line 537
of file em_lcd.h
.
References LCD.
__STATIC_INLINE void LCD_IntSet | ( | uint32_t | flags | ) |
Set one or more pending LCD interrupts from SW.
- Parameters
-
[in] flags
LCD interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the LCD module (LCD_IFS_nnn).
Definition at line 558
of file em_lcd.h
.
References LCD.
void LCD_SegmentRangeEnable | ( | LCD_SegmentRange_TypeDef | segmentRange, |
bool | enable |
||
) |
Enables updating this range of LCD segment lines.
- Parameters
-
[in] segmentRange
A range of 4 LCD segment lines to enable or disable for all enabled COM lines. [in] enable
Boolean true to enable segment updates, false to disable updates.
Definition at line 249
of file em_lcd.c
.
References LCD.
void LCD_SegmentSet | ( | int | com, |
int | bit, |
||
bool | enable |
||
) |
Turn on or clear a segment.
- Note
- For the Gecko Family, the maximum configuration is (COM-lines x Segment-Lines) 4x40. For the Tiny Gecko Family, the maximum configuration is 8x20 or 4x24. For the Giant Gecko Family, the maximum configuration is 8x36 or 4x40.
- Parameters
-
[in] com
A COM line to change. [in] bit
A bit index indicating which field to change. [in] enable
True will set segment, false will clear segment.
Definition at line 277
of file em_lcd.c
.
References BUS_RegBitWrite(), and LCD.
Referenced by displayBlock(), SegmentLCD_ARing(), SegmentLCD_Battery(), SegmentLCD_EnergyMode(), SegmentLCD_Number(), SegmentLCD_Symbol(), SegmentLCD_UnsignedHex(), and SegmentLCD_Write().
void LCD_SegmentSetHigh | ( | int | com, |
uint32_t | mask, |
||
uint32_t | bits |
||
) |
Update the high (32-39) segments on a given COM-line in one operation.
- Parameters
-
[in] com
Indicates a COM line to update. [in] mask
A bit mask for segments 32-39. [in] bits
A bit pattern for segments 32-39.
Definition at line 502
of file em_lcd.c
.
References LCD.
void LCD_SegmentSetLow | ( | int | com, |
uint32_t | mask, |
||
uint32_t | bits |
||
) |
Update 0-31 lowest segments on a given COM-line in one operation according to the bit mask.
- Parameters
-
[in] com
Indicates a COM line to update. [in] mask
A bit mask for segments 0-31. [in] bits
A bit pattern for segments 0-31.
Definition at line 413
of file em_lcd.c
.
References LCD.
__STATIC_INLINE void LCD_SyncBusyDelay | ( | uint32_t | flags | ) |
Polls LCD SYNCBUSY flags, until flag has been cleared.
- Parameters
-
[in] flags
Bit fields for LCD registers that will be updated before we continue.
Definition at line 500
of file em_lcd.h
.
References LCD.
Referenced by SegmentLCD_Disable(), SegmentLCD_Init(), SegmentLCD_Number(), SegmentLCD_UnsignedHex(), and SegmentLCD_Write().
__STATIC_INLINE uint32_t LCD_SyncBusyGet | ( | void |
| ) |
Returns SYNCBUSY bits, indicating which registers have pending updates.
- Returns
- Bit fields for LCD registers that have pending updates.
Definition at line 488
of file em_lcd.h
.
References LCD.
void LCD_UpdateCtrl | ( | LCD_UpdateCtrl_TypeDef | ud | ) |
Configure Update Control.
- Parameters
-
[in] ud
Configures the LCD update method.
Definition at line 161
of file em_lcd.c
.
References _LCD_CTRL_UDCTRL_MASK, and LCD.
void LCD_VBoostSet | ( | LCD_VBoostLevel_TypeDef | vboost | ) |
Configure voltage booster.
The resulting voltage level is described in each part number's data sheet
- Parameters
-
[in] vboost
Voltage boost level
Definition at line 632
of file em_lcd.c
.
References _LCD_DISPCTRL_VBLEV_MASK, and LCD.
Referenced by SegmentLCD_Init().
void LCD_VLCDSelect | ( | LCD_VLCDSel_TypeDef | vlcd | ) |
Select a source for VLCD.
- Parameters
-
[in] vlcd
Select a source for the VLCD voltage.
Definition at line 133
of file em_lcd.c
.
References _LCD_DISPCTRL_VLCDSEL_MASK, LCD, LCD_DISPCTRL_VLCDSEL_VDD, LCD_DISPCTRL_VLCDSEL_VEXTBOOST, lcdVLCDSelVDD, and lcdVLCDSelVExtBoost.
Referenced by SegmentLCD_Init().