EBI_TypeDef Struct ReferenceDevices > EFM32G_EBI
       Definition at line
       
        48
       
       of file
       
        efm32g_ebi.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | ADDRTIMING | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | POLARITY | 
| __IOM uint32_t | RDTIMING | 
| __IOM uint32_t | ROUTE | 
| __IOM uint32_t | WRTIMING | 
Field Documentation
| __IOM uint32_t EBI_TypeDef::ADDRTIMING | 
Address Timing Register
        Definition at line
        
         50
        
        of file
        
         efm32g_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         efm32g_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::POLARITY | 
Polarity Register
        Definition at line
        
         53
        
        of file
        
         efm32g_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::RDTIMING | 
Read Timing Register
        Definition at line
        
         51
        
        of file
        
         efm32g_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::ROUTE | 
I/O Routing Register
        Definition at line
        
         54
        
        of file
        
         efm32g_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::WRTIMING | 
Write Timing Register
        Definition at line
        
         52
        
        of file
        
         efm32g_ebi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/
       
efm32g_ebi.h