NORFLASH_Info_TypeDef Struct ReferenceKit Drivers > NorFlash
NORFLASH device information struct.
       Definition at line
       
        49
       
       of file
       
        norflash.h
       
       .
      
      
       #include <
       
     
        norflash.h
       
       >
      
         Data Fields | 
       |
| uint32_t | baseAddress | 
| uint32_t | deviceId | 
| uint32_t | deviceSize | 
| uint16_t | manufacturerId | 
| uint32_t | sectorCount | 
| uint32_t | sectorSize | 
Field Documentation
| uint32_t NORFLASH_Info_TypeDef::baseAddress | 
The device base address in cpu memory map.
        Definition at line
        
         50
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_AddressValid() , and NORFLASH_EraseDevice() .
| uint32_t NORFLASH_Info_TypeDef::deviceId | 
The device ID.
        Definition at line
        
         51
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::deviceSize | 
Total device size in bytes.
        Definition at line
        
         52
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_AddressValid() .
| uint16_t NORFLASH_Info_TypeDef::manufacturerId | 
The device manufacturer ID.
        Definition at line
        
         55
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::sectorCount | 
Number of sectors in the device.
        Definition at line
        
         53
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::sectorSize | 
Sector size in bytes.
        Definition at line
        
         54
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_EraseSector() , and NORFLASH_Program() .
The documentation for this struct was generated from the following files:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       
norflash.h - 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       
norflash_s29gl.h