EBI_Init_TypeDef Struct ReferenceEMLIB > EBI
EBI Initialization structure.
Definition at line
417
of file
em_ebi.h
.
#include <
em_ebi.h
>
Data Fields |
|
| uint32_t | addrHoldCycles |
| uint32_t | addrSetupCycles |
| EBI_Polarity_TypeDef | alePolarity |
| bool | ardyDisableTimeout |
| bool | ardyEnable |
| EBI_Polarity_TypeDef | ardyPolarity |
| uint32_t | banks |
| uint32_t | csLines |
| EBI_Polarity_TypeDef | csPolarity |
| bool | enable |
| EBI_Mode_TypeDef | mode |
| uint32_t | readHoldCycles |
| uint32_t | readSetupCycles |
| uint32_t | readStrobeCycles |
| EBI_Polarity_TypeDef | rePolarity |
| EBI_Polarity_TypeDef | wePolarity |
| uint32_t | writeHoldCycles |
| uint32_t | writeSetupCycles |
| uint32_t | writeStrobeCycles |
Field Documentation
| uint32_t EBI_Init_TypeDef::addrHoldCycles |
Number of cycles address is driven onto the ADDRDAT bus before ALE is asserted.
Definition at line
449
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::addrSetupCycles |
Number of cycles address is held after Address Latch Enable is asserted.
Definition at line
447
of file
em_ebi.h
.
Referenced by EBI_Init() .
| EBI_Polarity_TypeDef EBI_Init_TypeDef::alePolarity |
Address Latch Enable pin polarity, active high or low.
Definition at line
423
of file
em_ebi.h
.
Referenced by EBI_Init() .
| bool EBI_Init_TypeDef::ardyDisableTimeout |
Set to turn off 32 cycle timeout ability.
Definition at line
441
of file
em_ebi.h
.
Referenced by EBI_Init() .
| bool EBI_Init_TypeDef::ardyEnable |
Flag to enable or disable Address Ready support.
Definition at line
439
of file
em_ebi.h
.
Referenced by EBI_Init() .
| EBI_Polarity_TypeDef EBI_Init_TypeDef::ardyPolarity |
Address Ready pin polarity, active high or low.
Definition at line
421
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::banks |
Mask of flags which selects address banks to configure EBI_BANK<0-3>.
Definition at line
443
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::csLines |
Mask of flags which selects chip select lines to configure EBI_CS<0-3>.
Definition at line
445
of file
em_ebi.h
.
Referenced by EBI_Init() .
| EBI_Polarity_TypeDef EBI_Init_TypeDef::csPolarity |
Chip Select pin polarity, active high or low.
Definition at line
429
of file
em_ebi.h
.
Referenced by EBI_Init() .
| bool EBI_Init_TypeDef::enable |
Flag, if EBI should be enabled after configuration.
Definition at line
489
of file
em_ebi.h
.
Referenced by EBI_Init() .
| EBI_Mode_TypeDef EBI_Init_TypeDef::mode |
EBI operation mode, data, and address limits.
Definition at line
419
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::readHoldCycles |
Number of cycles CSn is held active after REn is deasserted.
Definition at line
459
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::readSetupCycles |
Number of cycles for address setup before REn is asserted.
Definition at line
455
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::readStrobeCycles |
Number of cycles REn is held active
Definition at line
457
of file
em_ebi.h
.
Referenced by EBI_Init() .
| EBI_Polarity_TypeDef EBI_Init_TypeDef::rePolarity |
Read Enable pin polarity, active high or low.
Definition at line
427
of file
em_ebi.h
.
Referenced by EBI_Init() .
| EBI_Polarity_TypeDef EBI_Init_TypeDef::wePolarity |
Write Enable pin polarity, active high or low.
Definition at line
425
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::writeHoldCycles |
Number of cycles CSn is held active after WEn is deasserted.
Definition at line
473
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::writeSetupCycles |
Number of cycles for address setup before WEn is asserted.
Definition at line
469
of file
em_ebi.h
.
Referenced by EBI_Init() .
| uint32_t EBI_Init_TypeDef::writeStrobeCycles |
Number of cycles WEn is held active
Definition at line
471
of file
em_ebi.h
.
Referenced by EBI_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_ebi.h