CALIBRATE_TypeDef Struct ReferenceDevices > EFM32G_CALIBRATE
       Definition at line
       
        49
       
       of file
       
        efm32g_calibrate.h
       
       .
      
         Data Fields | 
       |
| __IM uint32_t | ADDRESS | 
| __IM uint32_t | VALUE | 
Field Documentation
| __IM uint32_t CALIBRATE_TypeDef::ADDRESS | 
Address of calibration register
        Definition at line
        
         50
        
        of file
        
         efm32g_calibrate.h
        
        .
       
| __IM uint32_t CALIBRATE_TypeDef::VALUE | 
Default value for calibration register
        Definition at line
        
         51
        
        of file
        
         efm32g_calibrate.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/
       
efm32g_calibrate.h