Auto_ACK_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Auto acknowledge plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
struct | EZRADIODRV_AutoAckHandle |
EzRadio auto acknowledge plug-in instance initialization and handler structure.
|
|
Macros |
|
#define | EZRADIODRV_AUTO_ACK_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio auto acknowledge plug-in.
|
|
Typedefs |
|
typedef struct EZRADIODRV_AutoAckHandle | EZRADIODRV_AutoAckHandle_t |
EzRadio auto acknowledge plug-in instance initialization and handler structure.
|
|
typedef enum EZRADIODRV_AutoAckMode | EZRADIODRV_AutoAckMode_t |
EzRadio auto acknowledge mode.
|
|
typedef enum EZRADIODRV_AutoAckPacketMode | EZRADIODRV_AutoAckPacketMode_t |
EzRadio packet mode for auto acknowledge plug-in.
|
|
Enumerations |
|
enum |
EZRADIODRV_AutoAckMode
{
ezradiodrvAutoAckDisabled = 0, ezradiodrvAutoAckImmediate = 1, ezradiodrvAutoAckSkipOne = 2 } |
EzRadio auto acknowledge mode.
|
|
enum |
EZRADIODRV_AutoAckPacketMode
{
ezradiodrvAutoAckPktDefault = 0, ezradiodrvAutoAckPktCustom = 1 } |
EzRadio packet mode for auto acknowledge plug-in.
|
|
Functions |
|
void | ezradioDisableAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle) |
Disables auto acknowledge sending feature.
|
|
void | ezradioEnableAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle) |
Enables auto acknowledge sending feature.
|
|
void | ezradioSkipAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle) |
Configures auto acknowledge sending feature so that there will be no acknowledge transmitted to the next received packet. This is usefull is both nodes of a link uses auto acknowledgement.
|
|
Macro Definition Documentation
#define EZRADIODRV_AUTO_ACK_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio auto acknowledge plug-in.
Definition at line
92
of file
ezradio_auto_ack_plugin.h
.
Enumeration Type Documentation
EzRadio auto acknowledge mode.
Definition at line
65
of file
ezradio_auto_ack_plugin.h
.
EzRadio packet mode for auto acknowledge plug-in.
Definition at line
72
of file
ezradio_auto_ack_plugin.h
.
Function Documentation
void ezradioDisableAutoAck | ( | EZRADIODRV_AutoAckHandle_t * |
autoAckHandle
|
) |
Disables auto acknowledge sending feature.
- Parameters
-
autoAckHandle
Auto acknowledge plug-in handler.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
67
of file
ezradio_auto_ack_plugin.c
.
References EZRADIODRV_AutoAckHandle::ackMode , and ezradiodrvAutoAckDisabled .
void ezradioEnableAutoAck | ( | EZRADIODRV_AutoAckHandle_t * |
autoAckHandle
|
) |
Enables auto acknowledge sending feature.
- Parameters
-
autoAckHandle
Auto acknowledge plug-in handler.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
53
of file
ezradio_auto_ack_plugin.c
.
References EZRADIODRV_AutoAckHandle::ackMode , and ezradiodrvAutoAckImmediate .
void ezradioSkipAutoAck | ( | EZRADIODRV_AutoAckHandle_t * |
autoAckHandle
|
) |
Configures auto acknowledge sending feature so that there will be no acknowledge transmitted to the next received packet. This is usefull is both nodes of a link uses auto acknowledgement.
- Parameters
-
autoAckHandle
Auto acknowledge plug-in handler.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
83
of file
ezradio_auto_ack_plugin.c
.
References EZRADIODRV_AutoAckHandle::ackMode , and ezradiodrvAutoAckSkipOne .