MsdKit Drivers
Detailed Description
Implements USB Mass Storage Class (MSC).
MSC implementation for device.
The source code of the device implementation resides in kits/common/drivers/msdd.c and msdd.h
. The driver includes "msddmedia.h" to get the API definitions needed for media access. The drivers use the Bulk-Only Transport (BOT) mode of the MSC specification.
MSC device configuration options.
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file.
// USB interface number. Interfaces are numbered from zero to one less than // the number of concurrent interfaces supported by the configuration. // The interface number must be 0 for a standalone MSC device, for a // composite device which includes a MSC interface it must not be in conflict // with other device interfaces. #define MSD_INTERFACE_NO ( 0 ) // Endpoint address for data reception. #define MSD_BULK_OUT ( 0x01 ) // Endpoint address for data transmission. #define MSD_BULK_IN ( 0x81 )
Data Structures | |
struct | MSDBOT_CBW_TypeDef |
Bulk Only Transport (BOT) Command Block Wrapper (CBW) typedef. | |
struct | MSDBOT_CSW_TypeDef |
Bulk Only Transport (BOT) Command Status Wrapper (CSW) typedef. | |
struct | MSDD_CmdStatus_TypeDef |
Status info for one BOT CBW -> Data I/O -> CSW cycle. | |
struct | MSDSCSI_Inquiry_TypeDef |
SCSI Inquiry Command Descriptor Block (CDB) typedef. | |
struct | MSDSCSI_InquiryData_TypeDef |
SCSI Inquiry response data typedef. | |
struct | MSDSCSI_Read10_TypeDef |
SCSI Read 10 Command Descriptor Block (CDB) typedef. | |
struct | MSDSCSI_ReadCapacity_TypeDef |
SCSI Read Capacity Command Descriptor Block (CDB) typedef. | |
struct | MSDSCSI_ReadCapacityData_TypeDef |
SCSI Read Capacity response data typedef. | |
struct | MSDSCSI_RequestSense_TypeDef |
SCSI Request Sense Command Descriptor Block (CDB) typedef. | |
struct | MSDSCSI_RequestSenseData_TypeDef |
SCSI Request Sense response data typedef. | |
struct | MSDSCSI_StartStopUnit_TypeDef |
SCSI Start Stop Unit Command Descriptor Block (CDB) typedef. | |
struct | MSDSCSI_Verify10_TypeDef |
SCSI Verify 10 Command Descriptor Block (CDB) typedef. | |
struct | MSDSCSI_Write10_TypeDef |
SCSI Write 10 Command Descriptor Block (CDB) typedef. | |
Macros | |
#define | MEDIA_BUFSIZ 4096 |
#define | SCSI_INQUIRY 0x12 |
#define | SCSI_INQUIRYDATA_LEN 36U |
#define | SCSI_READ10 0x28 |
#define | SCSI_READ10_LEN 10U |
#define | SCSI_READCAPACITY 0x25 |
#define | SCSI_READCAPACITY_LEN 10U |
#define | SCSI_READCAPACITYDATA_LEN 8U |
#define | SCSI_REQUESTSENSE 0x03 |
#define | SCSI_REQUESTSENSE_LEN 6U |
#define | SCSI_REQUESTSENSEDATA_LEN 18U |
#define | SCSI_STARTSTOP_UNIT 0x1B |
#define | SCSI_STARTSTOPUNIT_LEN 6U |
#define | SCSI_TESTUNIT_READY 0x00 |
#define | SCSI_VERIFY10 0x2F |
#define | SCSI_VERIFY10_LEN 10U |
#define | SCSI_WRITE10 0x2A |
#define | SCSI_WRITE10_LEN 10U |
Enumerations | |
enum | MSDBOT_Status_TypeDef { MSDBOT_STATUS_OK = 0, MSDBOT_INIT_ERROR = -1, MSDBOT_CMD_FAILED = -2, MSDBOT_XFER_ERROR = -3 } |
MSDBOT status enumerator. | |
Functions | |
bool | MSDD_Handler (void) |
Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler. | |
void | MSDD_Init (int activityLedPort, uint32_t activityLedPin) |
Initialize MSD device. | |
int | MSDD_SetupCmd (const USB_Setup_TypeDef *setup) |
Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN". | |
void | MSDD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
Called whenever the USB device has changed its device state. | |
bool | MSDH_GetBlockSize (uint32_t *blockSize) |
Get blocksize from the device. | |
bool | MSDH_GetSectorCount (uint32_t *sectorCount) |
Get sectorcount from the device. | |
bool | MSDH_GetSectorSize (uint16_t *sectorSize) |
Get sectorsize from the device. | |
bool | MSDH_Init (uint8_t *usbDeviceInfo, int usbDeviceInfoSize) |
Initialize an USB connected Mass Storage Device. Checks if the device is a valid MSD device. Will perform all necessary MSD initialization. | |
bool | MSDH_ReadSectors (uint32_t lba, uint16_t sectors, void *data) |
Read sectors from device. | |
bool | MSDH_WriteSectors (uint32_t lba, uint16_t sectors, const void *data) |
Write sectors to device. | |
Macro Definition Documentation
#define MEDIA_BUFSIZ 4096 |
Intermediate media storage buffer size
Definition at line 32
of file msdd.h
.
#define SCSI_INQUIRY 0x12 |
SCSI Inquiry command opcode.
Definition at line 35
of file msdscsi.h
.
#define SCSI_INQUIRYDATA_LEN 36U |
SCSI Inquiry response data length.
Definition at line 45
of file msdscsi.h
.
Referenced by MSDD_Init(), MSDSCSI_Init(), and MSDSCSI_Inquiry().
#define SCSI_READ10 0x28 |
SCSI Read (10) command opcode.
Definition at line 38
of file msdscsi.h
.
#define SCSI_READ10_LEN 10U |
SCSI Read (10) CBD length.
Definition at line 42
of file msdscsi.h
.
Referenced by MSDD_Init(), and MSDSCSI_Init().
#define SCSI_READCAPACITY 0x25 |
SCSI Read Capacity command opcode.
Definition at line 37
of file msdscsi.h
.
#define SCSI_READCAPACITY_LEN 10U |
#define SCSI_READCAPACITYDATA_LEN 8U |
SCSI Read Capacity response data length.
Definition at line 50
of file msdscsi.h
.
Referenced by MSDD_Init(), MSDSCSI_Init(), and MSDSCSI_ReadCapacity().
#define SCSI_REQUESTSENSE 0x03 |
SCSI Request Sense command opcode.
Definition at line 34
of file msdscsi.h
.
#define SCSI_REQUESTSENSE_LEN 6U |
#define SCSI_REQUESTSENSEDATA_LEN 18U |
SCSI Request Sense response data length.
Definition at line 48
of file msdscsi.h
.
Referenced by MSDD_Init(), MSDSCSI_Init(), and MSDSCSI_RequestSense().
#define SCSI_STARTSTOP_UNIT 0x1B |
SCSI Start Stop Unit command opcode.
Definition at line 36
of file msdscsi.h
.
Referenced by MSDD_Handler().
#define SCSI_STARTSTOPUNIT_LEN 6U |
SCSI Start Stop Unit CDB length.
Definition at line 46
of file msdscsi.h
.
Referenced by MSDD_Init().
#define SCSI_TESTUNIT_READY 0x00 |
SCSI Test Unit Ready command opcode.
Definition at line 33
of file msdscsi.h
.
#define SCSI_VERIFY10 0x2F |
SCSI Verify (10) command opcode.
Definition at line 40
of file msdscsi.h
.
#define SCSI_VERIFY10_LEN 10U |
#define SCSI_WRITE10 0x2A |
SCSI Write (10) command opcode.
Definition at line 39
of file msdscsi.h
.
#define SCSI_WRITE10_LEN 10U |
SCSI Write (10) CDB length.
Definition at line 43
of file msdscsi.h
.
Referenced by MSDD_Init(), and MSDSCSI_Init().
Enumeration Type Documentation
Function Documentation
bool MSDD_Handler | ( | void |
| ) |
Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler.
- Returns
- Returns true if there is no pending tasks to perform. This means that energymodes (sleep) functionality can be used.
Definition at line 246
of file msdd.c
.
References MSDBOT_CBW_TypeDef::CBWCB, SCSI_STARTSTOP_UNIT, and SL_MIN.
void MSDD_Init | ( | int | activityLedPort, |
uint32_t | activityLedPin |
||
) |
Initialize MSD device.
- Parameters
-
[in] activityLedPort
Specify a GPIO port for a LED activity indicator (i.e. enum gpioPortX) Pass -1 if no indicator LED is available. [in] activityLedPin
Pin number on activityLedPort for the LED activity indicator.
Definition at line 204
of file msdd.c
.
References CMU_ClockEnable(), cmuClock_GPIO, GPIO_PinModeSet(), gpioModePushPull, SCSI_INQUIRYDATA_LEN, SCSI_READ10_LEN, SCSI_READCAPACITY_LEN, SCSI_READCAPACITYDATA_LEN, SCSI_REQUESTSENSE_LEN, SCSI_REQUESTSENSEDATA_LEN, SCSI_STARTSTOPUNIT_LEN, SCSI_VERIFY10_LEN, and SCSI_WRITE10_LEN.
int MSDD_SetupCmd | ( | const USB_Setup_TypeDef * | setup | ) |
Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN".
- Parameters
-
[in] setup
Pointer to an USB setup packet.
- Returns
- An appropriate status/error code. See USB_Status_TypeDef.
Definition at line 309
of file msdd.c
.
void MSDD_StateChangeEvent | ( | USBD_State_TypeDef | oldState, |
USBD_State_TypeDef | newState |
||
) |
Called whenever the USB device has changed its device state.
- Parameters
-
[in] oldState
The device USB state just leaved. See USBD_State_TypeDef. [in] newState
New (the current) USB device state. See USBD_State_TypeDef.
Definition at line 384
of file msdd.c
.
bool MSDH_GetBlockSize | ( | uint32_t * | blockSize | ) |
Get blocksize from the device.
- Note
- This function assumes that block size equals sector size.
- Parameters
-
[out] blockSize
The block size of device storage memory.
- Returns
- Returns true on success, false otherwise.
Definition at line 226
of file msdh.c
.
References MSDSCSI_ReadCapacity(), SL_ALIGN, and SL_ATTRIBUTE_ALIGN.
bool MSDH_GetSectorCount | ( | uint32_t * | sectorCount | ) |
Get sectorcount from the device.
- Parameters
-
[out] sectorCount
Number of sectors on the device.
- Returns
- Returns true on success, false otherwise.
Definition at line 175
of file msdh.c
.
References MSDSCSI_ReadCapacity(), SL_ALIGN, and SL_ATTRIBUTE_ALIGN.
bool MSDH_GetSectorSize | ( | uint16_t * | sectorSize | ) |
Get sectorsize from the device.
- Parameters
-
[out] sectorSize
The size of device sectors.
- Returns
- Returns true on success, false otherwise.
Definition at line 199
of file msdh.c
.
References MSDSCSI_ReadCapacity(), SL_ALIGN, and SL_ATTRIBUTE_ALIGN.
bool MSDH_Init | ( | uint8_t * | usbDeviceInfo, |
int | usbDeviceInfoSize |
||
) |
Initialize an USB connected Mass Storage Device. Checks if the device is a valid MSD device. Will perform all necessary MSD initialization.
- Note
- This function assumes that prior calls to USBH_Init() and USBH_WaitForDeviceConnectionB() have been performed. The contents of the usbDeviceInfo data buffer will be overwritten.
- Parameters
-
[in] usbDeviceInfo
Pointer to USB enumeration information. usbDeviceInfo must have been initialized by a prior call to USBH_WaitForDeviceConnectionB(). [in] usbDeviceInfoSize
The size of the usbDeviceInfo data buffer.
- Returns
- Returns true on success, false otherwise.
Definition at line 60
of file msdh.c
.
References MSDSCSI_Init(), MSDSCSI_Inquiry(), MSDSCSI_ReadCapacity(), MSDSCSI_RequestSense(), MSDSCSI_TestUnitReady(), SL_ALIGN, and SL_ATTRIBUTE_ALIGN.
bool MSDH_ReadSectors | ( | uint32_t | lba, |
uint16_t | sectors, |
||
void * | data |
||
) |
Read sectors from device.
- Parameters
-
[in] lba
Sector address (LBA) of first sector to read. [in] sectors
Number of sectors to read. [out] data
Data buffer through which data is returned to caller.
- Returns
- Returns true on success, false otherwise.
Definition at line 256
of file msdh.c
.
References MSDSCSI_Read10().
bool MSDH_WriteSectors | ( | uint32_t | lba, |
uint16_t | sectors, |
||
const void * | data |
||
) |
Write sectors to device.
- Parameters
-
[in] lba
Sector address (LBA) of first sector to write. [in] sectors
Number of sectors to write. [out] data
Data buffer containing data to be written.
- Returns
- Returns true on success, false otherwise.
Definition at line 277
of file msdh.c
.
References MSDSCSI_Write10().