tftdirect.c File Reference

EFM32GG_DK3750, TFT Initialization and setup for Direct Drive mode.

Version
5.6.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file tftdirect.c .

#include <stdbool.h>
#include " em_device.h "
#include " em_gpio.h "
#include " em_ebi.h "
#include " bsp.h "
#include " tftdirect.h "
#include " glib/glib.h "

Functions

void TFT_DirectGPIOConfig (void)
GPIO configuration for TFT direct drive.
bool TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit)
TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Variables

static bool runOnce = true

Variable Documentation

bool runOnce = true
static

Flag to indicate that we need to initialize once if starting up in

Definition at line 26 of file tftdirect.c .

Referenced by TFT_DirectInit() .