RTCCEMLIB

Detailed Description

Real Time Counter (RTCC) Peripheral API.

This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.

Data Structures

struct  RTCC_CCChConf_TypeDef
 
struct  RTCC_Init_TypeDef
 

Macros

#define RTCC_CC_NUM   3UL
 
#define RTCC_CH_INIT_CAPTURE_DEFAULT
 
#define RTCC_CH_INIT_COMPARE_DEFAULT
 
#define RTCC_CH_VALID(ch)    ((unsigned)(ch) < RTCC_CC_NUM)
 
#define RTCC_INIT_DEFAULT
 
#define rtccPRSCh0   0U
 
#define rtccPRSCh1   1U
 
#define rtccPRSCh10   10U
 
#define rtccPRSCh11   11U
 
#define rtccPRSCh2   2U
 
#define rtccPRSCh3   3U
 
#define rtccPRSCh4   4U
 
#define rtccPRSCh5   5U
 
#define rtccPRSCh6   6U
 
#define rtccPRSCh7   7U
 
#define rtccPRSCh8   8U
 
#define rtccPRSCh9   9U
 

Typedefs

typedef uint8_t RTCC_PRSSel_TypeDef
 

Enumerations

enum  RTCC_CapComChMode_TypeDef {
  rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF,
  rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE,
  rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE
}
 
enum  RTCC_CntMode_TypeDef {
  rtccCntModeNormal = _RTCC_CTRL_CNTMODE_NORMAL,
  rtccCntModeCalendar = _RTCC_CTRL_CNTMODE_CALENDAR
}
 
enum  RTCC_CntPresc_TypeDef {
  rtccCntPresc_1 = _RTCC_CTRL_CNTPRESC_DIV1,
  rtccCntPresc_2 = _RTCC_CTRL_CNTPRESC_DIV2,
  rtccCntPresc_4 = _RTCC_CTRL_CNTPRESC_DIV4,
  rtccCntPresc_8 = _RTCC_CTRL_CNTPRESC_DIV8,
  rtccCntPresc_16 = _RTCC_CTRL_CNTPRESC_DIV16,
  rtccCntPresc_32 = _RTCC_CTRL_CNTPRESC_DIV32,
  rtccCntPresc_64 = _RTCC_CTRL_CNTPRESC_DIV64,
  rtccCntPresc_128 = _RTCC_CTRL_CNTPRESC_DIV128,
  rtccCntPresc_256 = _RTCC_CTRL_CNTPRESC_DIV256,
  rtccCntPresc_512 = _RTCC_CTRL_CNTPRESC_DIV512,
  rtccCntPresc_1024 = _RTCC_CTRL_CNTPRESC_DIV1024,
  rtccCntPresc_2048 = _RTCC_CTRL_CNTPRESC_DIV2048,
  rtccCntPresc_4096 = _RTCC_CTRL_CNTPRESC_DIV4096,
  rtccCntPresc_8192 = _RTCC_CTRL_CNTPRESC_DIV8192,
  rtccCntPresc_16384 = _RTCC_CTRL_CNTPRESC_DIV16384,
  rtccCntPresc_32768 = _RTCC_CTRL_CNTPRESC_DIV32768
}
 
enum  RTCC_CompBase_TypeDef {
  rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT,
  rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT
}
 
enum  RTCC_CompMatchOutAction_TypeDef {
  rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE,
  rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE,
  rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR,
  rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET
}
 
enum  RTCC_DayCompareMode_TypeDef {
  rtccDayCompareModeMonth = _RTCC_CC_CTRL_DAYCC_MONTH,
  rtccDayCompareModeWeek = _RTCC_CC_CTRL_DAYCC_WEEK
}
 
enum  RTCC_InEdgeSel_TypeDef {
  rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING,
  rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING,
  rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH,
  rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE
}
 
enum  RTCC_PrescMode_TypeDef {
  rtccCntTickPresc = _RTCC_CTRL_CNTTICK_PRESC,
  rtccCntTickCCV0Match = _RTCC_CTRL_CNTTICK_CCV0MATCH
}
 

Functions

__STATIC_INLINE uint32_t RTCC_ChannelCaptureValueGet (int ch)
 Get RTCC input capture register value for selected channel.
 
__STATIC_INLINE uint32_t RTCC_ChannelCCVGet (int ch)
 Get RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function returns the compare value.
 
__STATIC_INLINE void RTCC_ChannelCCVSet (int ch, uint32_t value)
 Set RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function sets the compare value.
 
__STATIC_INLINE uint32_t RTCC_ChannelCompareValueGet (int ch)
 Get RTCC compare register value for selected channel.
 
__STATIC_INLINE void RTCC_ChannelCompareValueSet (int ch, uint32_t value)
 Set RTCC compare register value for selected channel.
 
__STATIC_INLINE uint32_t RTCC_ChannelDateGet (int ch)
 Get the calendar DATE register content for selected channel.
 
__STATIC_INLINE void RTCC_ChannelDateSet (int ch, uint32_t date)
 Set calendar DATE register for selected channel.
 
void RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const *confPtr)
 Configure the selected capture/compare channel of the RTCC.
 
__STATIC_INLINE uint32_t RTCC_ChannelTimeGet (int ch)
 Get calendar TIME register content for selected channel.
 
__STATIC_INLINE void RTCC_ChannelTimeSet (int ch, uint32_t time)
 Set calendar TIME register for selected channel.
 
__STATIC_INLINE uint32_t RTCC_CombinedCounterGet (void)
 Get combined CNT/PRECNT register content.
 
__STATIC_INLINE uint32_t RTCC_CounterGet (void)
 Get RTCC counter value.
 
__STATIC_INLINE void RTCC_CounterSet (uint32_t value)
 Set RTCC CNT counter.
 
__STATIC_INLINE uint32_t RTCC_DateGet (void)
 Get DATE register value.
 
__STATIC_INLINE void RTCC_DateSet (uint32_t date)
 Set RTCC DATE register.
 
__STATIC_INLINE void RTCC_EM4WakeupEnable (bool enable)
 Enable/disable EM4 wakeup capability.
 
void RTCC_Enable (bool enable)
 Enable/disable RTCC counting.
 
void RTCC_Init (const RTCC_Init_TypeDef *init)
 Initialize RTCC.
 
__STATIC_INLINE void RTCC_IntClear (uint32_t flags)
 Clear one or more pending RTCC interrupts.
 
__STATIC_INLINE void RTCC_IntDisable (uint32_t flags)
 Disable one or more RTCC interrupts.
 
__STATIC_INLINE void RTCC_IntEnable (uint32_t flags)
 Enable one or more RTCC interrupts.
 
__STATIC_INLINE uint32_t RTCC_IntGet (void)
 Get pending RTCC interrupt flags.
 
__STATIC_INLINE uint32_t RTCC_IntGetEnabled (void)
 Get enabled and pending RTCC interrupt flags.
 
__STATIC_INLINE void RTCC_IntSet (uint32_t flags)
 Set one or more pending RTCC interrupts from SW.
 
__STATIC_INLINE void RTCC_Lock (void)
 Lock RTCC registers.
 
__STATIC_INLINE uint32_t RTCC_PreCounterGet (void)
 Get RTCC pre-counter value.
 
__STATIC_INLINE void RTCC_PreCounterSet (uint32_t preCntVal)
 Set RTCC pre-counter value.
 
void RTCC_Reset (void)
 Restore RTCC to its reset state.
 
__STATIC_INLINE void RTCC_RetentionRamPowerDown (void)
 Power down retention RAM.
 
void RTCC_StatusClear (void)
 Clear the STATUS register.
 
__STATIC_INLINE uint32_t RTCC_StatusGet (void)
 Get STATUS register value.
 
__STATIC_INLINE uint32_t RTCC_TimeGet (void)
 Get TIME register value.
 
__STATIC_INLINE void RTCC_TimeSet (uint32_t time)
 Set RTCC TIME register.
 
__STATIC_INLINE void RTCC_Unlock (void)
 Unlock RTCC registers.
 

Macro Definition Documentation

#define RTCC_CC_NUM   3UL

Number of RTCC capture/compare channels

Definition at line 385 of file em_rtcc.h.

Referenced by RTCC_Reset().

#define RTCC_CH_INIT_CAPTURE_DEFAULT
Value:
{ \
rtccCapComChModeCapture, /* Select input capture mode. */ \
rtccCompMatchOutActionPulse, /* Create pulse on capture. */ \
0, /* PRS channel 0. */ \
rtccInEdgeRising, /* Rising edge detection. */ \
rtccCompBaseCnt, /* Don't care. */ \
0, /* Don't care. */ \
rtccDayCompareModeMonth /* Don't care */ \
}

Default RTCC channel input capture initialization structure.

Definition at line 370 of file em_rtcc.h.

#define RTCC_CH_INIT_COMPARE_DEFAULT
Value:
{ \
rtccCapComChModeCompare, /* Select output compare mode. */ \
rtccCompMatchOutActionPulse, /* Create pulse on compare match.*/ \
0, /* PRS channel 0 (not used). */ \
rtccInEdgeNone, /* No edge detection. */ \
rtccCompBaseCnt, /* Counter comparison base. */ \
0, /* No compare mask bits set. */ \
rtccDayCompareModeMonth /* Don't care */ \
}

Default RTCC channel output compare initialization structure.

Definition at line 358 of file em_rtcc.h.

#define RTCC_CH_VALID (   ch)    ((unsigned)(ch) < RTCC_CC_NUM)

Validation of valid RTCC channel for assert statements.

Definition at line 389 of file em_rtcc.h.

Referenced by RTCC_ChannelCaptureValueGet(), RTCC_ChannelCompareValueGet(), RTCC_ChannelCompareValueSet(), RTCC_ChannelDateGet(), RTCC_ChannelDateSet(), RTCC_ChannelInit(), RTCC_ChannelTimeGet(), and RTCC_ChannelTimeSet().

#define RTCC_INIT_DEFAULT
Value:
{ \
true, /* Start counting when initialization is done. */ \
false, /* Disable RTCC during debug halt. */ \
false, /* Disable pre-counter wrap on ch. 0 CCV value. */ \
false, /* Disable counter wrap on ch. 1 CCV value. */ \
rtccCntPresc_32, /* 977 us per tick. */ \
rtccCntTickPresc, /* Counter increments according to prescaler value.*/ \
false, /* No RTCC oscillator failure detection. */ \
rtccCntModeNormal, /* Normal RTCC mode. */ \
false, /* No leap year correction. */ \
}

Default RTCC initialization structure.

Definition at line 319 of file em_rtcc.h.

Referenced by UDELAY_Calibrate().

#define rtccPRSCh0   0U

Deprecated PRS channel values. New code should use an integer instead of using these deprecated enum values.

Definition at line 171 of file em_rtcc.h.

Typedef Documentation

typedef uint8_t RTCC_PRSSel_TypeDef

PRS channel number. This type is used when configuring input capture mode on a RTCC channel.

Definition at line 167 of file em_rtcc.h.

Enumeration Type Documentation

Capture/Compare channel mode.

Enumerator
rtccCapComChModeOff 

Capture/Compare channel turned off.

rtccCapComChModeCapture 

Capture mode.

rtccCapComChModeCompare 

Compare mode.

Definition at line 151 of file em_rtcc.h.

Operational mode of the counter.

Enumerator
rtccCntModeNormal 

Normal counter mode. The counter is incremented by 1 for each tick.

rtccCntModeCalendar 

Calendar mode. Refer to the RTCC chapter of the Reference Manual for more details on the calendar mode.

Definition at line 76 of file em_rtcc.h.

Counter prescaler selection.

Enumerator
rtccCntPresc_1 

Divide clock by 1.

rtccCntPresc_2 

Divide clock by 2.

rtccCntPresc_4 

Divide clock by 4.

rtccCntPresc_8 

Divide clock by 8.

rtccCntPresc_16 

Divide clock by 16.

rtccCntPresc_32 

Divide clock by 32.

rtccCntPresc_64 

Divide clock by 64.

rtccCntPresc_128 

Divide clock by 128.

rtccCntPresc_256 

Divide clock by 256.

rtccCntPresc_512 

Divide clock by 512.

rtccCntPresc_1024 

Divide clock by 1024.

rtccCntPresc_2048 

Divide clock by 2048.

rtccCntPresc_4096 

Divide clock by 4096.

rtccCntPresc_8192 

Divide clock by 8192.

rtccCntPresc_16384 

Divide clock by 16384.

rtccCntPresc_32768 

Divide clock by 32768.

Definition at line 88 of file em_rtcc.h.

Capture/Compare channel compare mode.

Enumerator
rtccCompBaseCnt 

CCVx is compared with the CNT register.

rtccCompBasePreCnt 

CCVx is compared with a CNT[16:0] and PRECNT[14:0].

Definition at line 193 of file em_rtcc.h.

Compare match output action mode.

Enumerator
rtccCompMatchOutActionPulse 

Generate a pulse.

rtccCompMatchOutActionToggle 

Toggle output.

rtccCompMatchOutActionClear 

Clear output.

rtccCompMatchOutActionSet 

Set output.

Definition at line 158 of file em_rtcc.h.

Day compare mode.

Enumerator
rtccDayCompareModeMonth 

Day of month is selected for Capture/Compare.

rtccDayCompareModeWeek 

Day of week is selected for Capture/Compare.

Definition at line 203 of file em_rtcc.h.

Input edge select.

Enumerator
rtccInEdgeRising 

Rising edges detected.

rtccInEdgeFalling 

Falling edges detected.

rtccInEdgeBoth 

Both edges detected.

rtccInEdgeNone 

No edge detection, signal is left as is.

Definition at line 185 of file em_rtcc.h.

Prescaler mode of the RTCC counter.

Enumerator
rtccCntTickPresc 

CNT register ticks according to prescaler value.

rtccCntTickCCV0Match 

CNT register ticks when PRECNT matches the 15 least significant bits of ch. 0 CCV register.

Definition at line 130 of file em_rtcc.h.

Function Documentation

__STATIC_INLINE uint32_t RTCC_ChannelCaptureValueGet ( int  ch)

Get RTCC input capture register value for selected channel.

Parameters
[in]chChannel selector.
Returns
Capture register value.

Definition at line 445 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE uint32_t RTCC_ChannelCCVGet ( int  ch)

Get RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function returns the compare value.

Parameters
[in]chChannel selector.
Returns
Capture/compare register value.

Definition at line 467 of file em_rtcc.h.

References RTCC_ChannelCompareValueGet().

__STATIC_INLINE void RTCC_ChannelCCVSet ( int  ch,
uint32_t  value 
)

Set RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function sets the compare value.

Parameters
[in]chChannel selector.
[in]valueCapture/compare register value

Definition at line 484 of file em_rtcc.h.

References RTCC_ChannelCompareValueSet().

__STATIC_INLINE uint32_t RTCC_ChannelCompareValueGet ( int  ch)

Get RTCC compare register value for selected channel.

Parameters
[in]chChannel selector.
Returns
Compare register value.

Definition at line 405 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

Referenced by RTCC_ChannelCCVGet().

__STATIC_INLINE void RTCC_ChannelCompareValueSet ( int  ch,
uint32_t  value 
)

Set RTCC compare register value for selected channel.

Parameters
[in]chChannel selector.
[in]valueCompare register value

Definition at line 425 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

Referenced by RTCC_ChannelCCVSet().

__STATIC_INLINE uint32_t RTCC_ChannelDateGet ( int  ch)

Get the calendar DATE register content for selected channel.

Parameters
[in]chChannel selector.
Returns
DATE register value.

Definition at line 500 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE void RTCC_ChannelDateSet ( int  ch,
uint32_t  date 
)

Set calendar DATE register for selected channel.

Parameters
[in]chChannel selector.
[in]dateDATE value.

Definition at line 516 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

void RTCC_ChannelInit ( int  ch,
RTCC_CCChConf_TypeDef const *  confPtr 
)

Configure the selected capture/compare channel of the RTCC.

Use this function to configure an RTCC channel. Select capture/compare mode, match output action, overflow output action, and PRS input configuration. See the configuration structure RTCC_CCChConf_TypeDef for more details.

Parameters
[in]chA channel selector.
[in]confPtrA pointer to the configuration structure.

Configure the selected capture/compare channel.

Definition at line 80 of file em_rtcc.c.

References _RTCC_CC_CTRL_CMOA_SHIFT, _RTCC_CC_CTRL_COMPBASE_SHIFT, _RTCC_CC_CTRL_COMPMASK_MASK, _RTCC_CC_CTRL_COMPMASK_SHIFT, _RTCC_CC_CTRL_DAYCC_SHIFT, _RTCC_CC_CTRL_ICEDGE_SHIFT, _RTCC_CC_CTRL_MODE_SHIFT, _RTCC_CC_CTRL_PRSSEL_SHIFT, RTCC_CCChConf_TypeDef::chMode, RTCC_CCChConf_TypeDef::compBase, RTCC_CCChConf_TypeDef::compMask, RTCC_CCChConf_TypeDef::compMatchOutAction, RTCC_CCChConf_TypeDef::dayCompMode, RTCC_CCChConf_TypeDef::inputEdgeSel, PRS, RTCC_CCChConf_TypeDef::prsSel, RTCC, RTCC_CH_VALID, and rtccCapComChModeCapture.

Referenced by RTCDRV_Init().

__STATIC_INLINE uint32_t RTCC_ChannelTimeGet ( int  ch)

Get calendar TIME register content for selected channel.

Parameters
[in]chChannel selector.
Returns
TIME register value.

Definition at line 532 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE void RTCC_ChannelTimeSet ( int  ch,
uint32_t  time 
)

Set calendar TIME register for selected channel.

Parameters
[in]chChannel selector.
[in]timeTIME value.

Definition at line 548 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE uint32_t RTCC_CombinedCounterGet ( void  )

Get combined CNT/PRECNT register content.

Returns
CNT/PRECNT register value.

Definition at line 562 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_CounterGet ( void  )

Get RTCC counter value.

Returns
Current RTCC counter value.

Definition at line 579 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_CounterSet ( uint32_t  value)

Set RTCC CNT counter.

Parameters
[in]valueCNT value.

Definition at line 596 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_DateGet ( void  )

Get DATE register value.

Returns
Current DATE register value.

Definition at line 615 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_DateSet ( uint32_t  date)

Set RTCC DATE register.

Parameters
[in]dateDATE value.

Definition at line 627 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_EM4WakeupEnable ( bool  enable)

Enable/disable EM4 wakeup capability.

Parameters
[in]enableSet to true to enable EM4 wakeup, set to false otherwise.

Definition at line 641 of file em_rtcc.h.

References RTCC, and RTCC_EM4WUEN_EM4WU.

void RTCC_Enable ( bool  enable)

Enable/disable RTCC counting.

Parameters
[in]enableTrue to enable RTCC counting, false to disable counting.

Definition at line 118 of file em_rtcc.c.

References _RTCC_CTRL_ENABLE_SHIFT, BUS_RegBitWrite(), and RTCC.

Referenced by RTCDRV_DeInit(), and UDELAY_Calibrate().

void RTCC_Init ( const RTCC_Init_TypeDef init)

Initialize RTCC.

Note that the compare values must be set separately with RTCC_CompareSet(), which should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.

Parameters
[in]initA pointer to the RTCC initialization structure.

Definition at line 158 of file em_rtcc.c.

References _RTCC_CTRL_CCV1TOP_SHIFT, _RTCC_CTRL_CNTMODE_SHIFT, _RTCC_CTRL_CNTPRESC_SHIFT, _RTCC_CTRL_CNTTICK_SHIFT, _RTCC_CTRL_DEBUGRUN_SHIFT, _RTCC_CTRL_ENABLE_SHIFT, _RTCC_CTRL_LYEARCORRDIS_SHIFT, _RTCC_CTRL_OSCFDETEN_SHIFT, _RTCC_CTRL_PRECCV0TOP_SHIFT, RTCC_Init_TypeDef::cntMode, RTCC_Init_TypeDef::cntWrapOnCCV1, RTCC_Init_TypeDef::debugRun, RTCC_Init_TypeDef::disLeapYearCorr, RTCC_Init_TypeDef::enable, RTCC_Init_TypeDef::enaOSCFailDetect, RTCC_Init_TypeDef::precntWrapOnCCV0, RTCC_Init_TypeDef::presc, RTCC_Init_TypeDef::prescMode, and RTCC.

Referenced by RTCDRV_Init(), and UDELAY_Calibrate().

__STATIC_INLINE void RTCC_IntClear ( uint32_t  flags)

Clear one or more pending RTCC interrupts.

Parameters
[in]flagsRTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.

Definition at line 665 of file em_rtcc.h.

References RTCC.

Referenced by RTCC_Reset().

__STATIC_INLINE void RTCC_IntDisable ( uint32_t  flags)

Disable one or more RTCC interrupts.

Parameters
[in]flagsRTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.

Definition at line 682 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_IntEnable ( uint32_t  flags)

Enable one or more RTCC interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTCC_IntClear() prior to enabling the interrupt.
Parameters
[in]flagsRTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.

Definition at line 700 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_IntGet ( void  )

Get pending RTCC interrupt flags.

Note
Event bits are not cleared by using this function.
Returns
Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Definition at line 716 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_IntGetEnabled ( void  )

Get enabled and pending RTCC interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Returns
Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Definition at line 732 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_IntSet ( uint32_t  flags)

Set one or more pending RTCC interrupts from SW.

Parameters
[in]flagsRTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).

Definition at line 750 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_Lock ( void  )

Lock RTCC registers.

Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.

Definition at line 768 of file em_rtcc.h.

References CMU, CMU_LOCK_LOCKKEY_LOCK, CMU_LOCK_LOCKKEY_LOCKED, CMU_LOCK_LOCKKEY_UNLOCK, RTCC, and RTCC_LOCK_LOCKKEY_UNLOCK.

__STATIC_INLINE uint32_t RTCC_PreCounterGet ( void  )

Get RTCC pre-counter value.

Returns
Current RTCC pre-counter value.

Definition at line 797 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_PreCounterSet ( uint32_t  preCntVal)

Set RTCC pre-counter value.

Parameters
[in]preCntValRTCC pre-counter value to be set.

Definition at line 814 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_RetentionRamPowerDown ( void  )

Power down retention RAM.

Note
Once retention RAM is powered down, it cannot be powered up again.

Definition at line 835 of file em_rtcc.h.

References RTCC, and RTCC_POWERDOWN_RAM.

__STATIC_INLINE uint32_t RTCC_StatusGet ( void  )

Get STATUS register value.

Returns
Current STATUS register value.

Definition at line 854 of file em_rtcc.h.

References RTCC, and RTCC_SYNCBUSY_CMD.

__STATIC_INLINE uint32_t RTCC_TimeGet ( void  )

Get TIME register value.

Returns
Current TIME register value.

Definition at line 928 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_TimeSet ( uint32_t  time)

Set RTCC TIME register.

Parameters
[in]timeTIME value.

Definition at line 940 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_Unlock ( void  )

Unlock RTCC registers.

Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.

Definition at line 955 of file em_rtcc.h.

References CMU, CMU_LOCK_LOCKKEY_LOCK, CMU_LOCK_LOCKKEY_LOCKED, CMU_LOCK_LOCKKEY_UNLOCK, RTCC, and RTCC_LOCK_LOCKKEY_UNLOCK.

Referenced by RTCC_Reset().