MSDSCSI_RequestSense_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD

SCSI Request Sense Command Descriptor Block (CDB) typedef.

Definition at line 128 of file msdscsi.h .

#include < msdscsi.h >

Data Fields

struct {
uint8_t Desc : 1
uint8_t Reserved1 : 7
};
uint8_t AllocationLength
uint8_t Control
uint8_t OpCode
uint8_t Reserved2
uint8_t Reserved3

Field Documentation

uint8_t MSDSCSI_RequestSense_TypeDef::AllocationLength

Number of sense data bytes requested.

Definition at line 136 of file msdscsi.h .

uint8_t MSDSCSI_RequestSense_TypeDef::Control

Control byte.

Definition at line 137 of file msdscsi.h .

uint8_t MSDSCSI_RequestSense_TypeDef::Desc

Descriptor format.

Definition at line 131 of file msdscsi.h .

uint8_t MSDSCSI_RequestSense_TypeDef::OpCode

Command opcode.

Definition at line 129 of file msdscsi.h .

uint8_t MSDSCSI_RequestSense_TypeDef::Reserved1

Reserved, expect 0.

Definition at line 132 of file msdscsi.h .

uint8_t MSDSCSI_RequestSense_TypeDef::Reserved2

Reserved, expect 0.

Definition at line 134 of file msdscsi.h .

uint8_t MSDSCSI_RequestSense_TypeDef::Reserved3

Reserved, expect 0.

Definition at line 135 of file msdscsi.h .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/hardware/kit/common/drivers/ msdscsi.h