__BMP_Header Struct ReferencePlatform Middleware > GLIB
BMP Module header structure. Must be packed to exact 54 bytes.
Definition at line 86
of file bmp.h
.
#include <
bmp.h
>
Data Fields | |
uint16_t | bitsPerPixel |
uint16_t | colorPlanes |
uint32_t | colorsRequired |
uint32_t | colorsUsed |
uint32_t | compressionType |
uint32_t | dataOffset |
uint32_t | fileSize |
uint32_t | headerSize |
uint32_t | height |
uint32_t | hPixelsPerMeter |
uint32_t | imageDataSize |
uint16_t | magic |
uint16_t | reserved1 |
uint16_t | reserved2 |
uint32_t | vPixelsPerMeter |
uint32_t | width |
Field Documentation
uint16_t __BMP_Header::bitsPerPixel |
Color depth
Definition at line 110
of file bmp.h
.
Referenced by BMP_getBitsPerPixel(), BMP_readRawData(), BMP_readRgbData(), and BMP_reset().
uint16_t __BMP_Header::colorPlanes |
Color planes
Definition at line 108
of file bmp.h
.
uint32_t __BMP_Header::colorsRequired |
Number of color indices that are required for displaying the bitmap
Definition at line 122
of file bmp.h
.
uint32_t __BMP_Header::colorsUsed |
Number of color indices in the color table that are actually used by the bitmap
Definition at line 120
of file bmp.h
.
uint32_t __BMP_Header::compressionType |
Compression type
Definition at line 112
of file bmp.h
.
Referenced by BMP_getCompressionType(), BMP_readRawData(), BMP_readRgbData(), and BMP_reset().
uint32_t __BMP_Header::dataOffset |
Data offset relative to the start of the bmp data
Definition at line 100
of file bmp.h
.
Referenced by BMP_getDataOffset(), and BMP_reset().
uint32_t __BMP_Header::fileSize |
Size of the bmp file in bytes
Definition at line 94
of file bmp.h
.
Referenced by BMP_getFileSize(), and BMP_reset().
uint32_t __BMP_Header::headerSize |
uint32_t __BMP_Header::height |
Height of bmp
Definition at line 106
of file bmp.h
.
Referenced by BMP_getHeight(), BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRgbData(), and BMP_reset().
uint32_t __BMP_Header::hPixelsPerMeter |
Horizontal resolution (pixels per meter)
Definition at line 116
of file bmp.h
.
uint32_t __BMP_Header::imageDataSize |
Size of raw BMP data
Definition at line 114
of file bmp.h
.
Referenced by BMP_getImageDataSize(), BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRgbData(), and BMP_reset().
uint16_t __BMP_Header::magic |
Magic identifier: "BM" (for bmp files)
Definition at line 92
of file bmp.h
.
Referenced by BMP_reset().
uint16_t __BMP_Header::reserved1 |
Reserved 1
Definition at line 96
of file bmp.h
.
uint16_t __BMP_Header::reserved2 |
Reserved 2
Definition at line 98
of file bmp.h
.
uint32_t __BMP_Header::vPixelsPerMeter |
Vertical resolution (pixels per meter)
Definition at line 118
of file bmp.h
.
uint32_t __BMP_Header::width |
Width of bmp
Definition at line 104
of file bmp.h
.
Referenced by BMP_getWidth(), BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), and BMP_readRgbData().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/middleware/glib/glib/
bmp.h