CORE_nvicMask_t Struct ReferenceEMLIB > CORE

Storage for NVIC interrupt masks.

Definition at line 222 of file em_core.h .

#include < em_core.h >

Data Fields

uint32_t a [ CORE_NVIC_REG_WORDS ]

Field Documentation

uint32_t CORE_nvicMask_t::a[ CORE_NVIC_REG_WORDS ]

Array of NVIC mask words.

Definition at line 223 of file em_core.h .

Referenced by CORE_GetNvicMaskDisableState() , CORE_NvicIRQDisabled() , CORE_NvicMaskClearIRQ() , CORE_NvicMaskSetIRQ() , and CORE_YieldNvicMask() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_core.h