EZRADIODRV_AutoAckHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Auto_ACK_Plugin

EzRadio auto acknowledge plug-in instance initialization and handler structure.

Definition at line 63 of file ezradio_auto_ack_plugin.h.

#include <ezradio_auto_ack_plugin.h>

Data Fields

EZRADIODRV_AutoAckMode_t ackMode
 Auto ack mode.
 
EZRADIODRV_PacketLengthConfig_t lenConfig
 Pakcet length config for auto ack.
 
uint8_t * pktBuf
 Pointer to the buffer that holds the auto ack packet.
 
uint16_t pktId
 Auto ack packet ID.
 
EZRADIODRV_AutoAckPacketMode_t pktMode
 Packet mode for aut ack.
 
EZRADIODRV_Callback_t userCallback
 User callback.
 

The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emdrv/ezradiodrv/plugins/inc/ezradio_auto_ack_plugin.h