MSDSCSI_InquiryData_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
SCSI Inquiry response data typedef.
Definition at line 75
of file msdscsi.h
.
#include <
msdscsi.h
>
Data Fields | |
struct { | |
uint8_t PeripheralDeviceType: 5 | |
uint8_t PeripheralQualifier: 3 | |
}; | |
struct { | |
uint8_t Removable: 1 | |
uint8_t Reserved1: 7 | |
}; | |
struct { | |
uint8_t HiSup: 1 | |
uint8_t NormACA: 1 | |
uint8_t Obsolete1: 2 | |
uint8_t ResponseDataFormat: 4 | |
}; | |
struct { | |
uint8_t Acc: 1 | |
uint8_t Protect: 1 | |
uint8_t Reserved2: 2 | |
uint8_t Sccs: 1 | |
uint8_t ThirdPartyCode: 1 | |
uint8_t Tpgs: 2 | |
}; | |
struct { | |
uint8_t Addr16: 1 | |
uint8_t BQue: 1 | |
uint8_t EncServ: 1 | |
uint8_t MChngr: 1 | |
uint8_t MultiP: 1 | |
uint8_t Obsolete2: 2 | |
uint8_t Vs1: 1 | |
}; | |
struct { | |
uint8_t CmdQue: 1 | |
uint8_t Linked: 1 | |
uint8_t Obsolete3: 1 | |
uint8_t Obsolete4: 2 | |
uint8_t Sync: 1 | |
uint8_t Vs2: 1 | |
uint8_t Wbus16: 1 | |
}; | |
uint8_t | AdditionalLength |
uint8_t | ProductId [16] |
uint8_t | ProductRevisionLevel [4] |
uint8_t | T10VendorId [8] |
uint8_t | Version |
Field Documentation
uint8_t MSDSCSI_InquiryData_TypeDef::Acc |
Access Controls Coordinator.
Definition at line 97
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::AdditionalLength |
Number of additional inquiry bytes that follow.
Definition at line 91
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Addr16 |
Wide SCSI address support.
Definition at line 101
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::BQue |
Full/Basic task management model.
Definition at line 107
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::CmdQue |
Command queueing support.
Definition at line 111
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::EncServ |
Enclosure Services support.
Definition at line 106
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::HiSup |
Hierarchical Support indicator.
Definition at line 87
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Linked |
Linked commands support.
Definition at line 113
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::MChngr |
Medium Changer indicator.
Definition at line 103
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::MultiP |
Multi Port indicator.
Definition at line 104
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::NormACA |
Normal Auto Contingent Allegiance support.
Definition at line 88
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Obsolete1 |
Obsolete, expect any value.
Definition at line 89
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Obsolete2 |
Obsolete, expect any value.
Definition at line 102
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Obsolete3 |
Obsolete, expect any value.
Definition at line 112
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Obsolete4 |
Obsolete, expect any value.
Definition at line 116
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::PeripheralDeviceType |
Peripheral device type .
Definition at line 77
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::PeripheralQualifier |
Peripheral qualifier.
Definition at line 78
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::ProductId[16] |
Product ID, 16 ASCII codes.
Definition at line 119
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::ProductRevisionLevel[4] |
Product revision level, 4 ASCII codes.
Definition at line 120
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Protect |
Protection information support.
Definition at line 93
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Removable |
Removable medium indicator.
Definition at line 82
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Reserved1 |
Reserved, expect 0.
Definition at line 81
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Reserved2 |
Reserved, expect 0.
Definition at line 94
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::ResponseDataFormat |
Response data format value.
Definition at line 86
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Sccs |
SCSI Controller Commands Supported.
Definition at line 98
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Sync |
Synchronous data transfer support.
Definition at line 114
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::T10VendorId[8] |
T10 Vendor ID, 8 ASCII codes.
Definition at line 118
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::ThirdPartyCode |
Third Party copy command support.
Definition at line 95
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Tpgs |
Target Port Group Support.
Definition at line 96
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Version |
SPC standard version implementation.
Definition at line 84
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Vs1 |
Vendor specific.
Definition at line 105
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Vs2 |
Vendor specific.
Definition at line 110
of file msdscsi.h
.
uint8_t MSDSCSI_InquiryData_TypeDef::Wbus16 |
Wide SCSI data transfer support.
Definition at line 115
of file msdscsi.h
.
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/
msdscsi.h