Kit Drivers
Detailed Description
Kit support and drivers.
Drivers and support modules for board components such as displays, sensors and memory components on EFM32, EZR32 and EFR32 kits.
For display device support, see section Display Device Driver Stack for more information.
Modules | |
CPT112S_I2C | |
Silicon Labs 12-pad Capacitive Touch Evaluation Board I2C driver. | |
CapSense | |
Capacitive sensing driver. | |
Display | |
Display device driver stack library. | |
DmaCtrl | |
uDMA control block array. | |
EEPROM | |
I2C EEPROM Driver. | |
Gecko USB MSD | |
USB Mass Storage Class (MSC). | |
Gecko USB RS232 bridge | |
Gecko USB to RS232 bridge (CDC Class). | |
HidKeyboard | |
Implements a USB HID class keyboard. | |
I2CSPM | |
I2C Simple Polled Master driver. | |
Ksz8851snl | |
KSZ8851SNL SPI Ethernet Controller driver. | |
MicroSd | |
SPI driver for micro SD card. | |
NANDFlash | |
Driver for Numonyx NAND256W3A NAND Flash devices. | |
NORFlash | |
Driver for Spanion S29GL128P90FFIR13 and S29GL064N NOR Flash devices. | |
RetargetIo | |
Standard I/O retargeting driver. | |
SL_EFPDRV | |
EFP (Energy Friendly PMIC) driver. | |
SegmentLcd | |
Segment LCD driver. | |
Si114x | |
Silicon Labs Si114x Ultraviolet (UV) Index, Gesture, Proximity, and Ambient Light Sensor I2C driver. | |
Si7013 | |
Silicon Labs Si7013 Relative Humidity and Temperature Sensor I2C driver. | |
Si72xx | |
Silicon Labs Si72xx Magnetic Hall Effect Sensor I2C driver. | |
TFT | |
Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode. | |
TempSensor | |
Driver for DS75 I2C temperature sensor. | |
Textdisplay | |
Line based text output terminal interface on top of the DISPLAY device driver stack. See TextDisplay Library for more information. | |
Touch | |
Touch panel driver for DK3650, DK3750 and DK3850 Development Kits. | |
Udelay | |
Calibrated busy wait loop. | |
UsbHid | |
USB HID keyboard scan codes. | |
VddCheck | |
VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API. | |