USART_InitAsync_TypeDef Struct ReferenceEMLIB > USART

Asynchronous mode initialization structure.

Definition at line 282 of file em_usart.h.

#include <em_usart.h>

Data Fields

bool autoCsEnable
 
uint32_t baudrate
 
USART_Databits_TypeDef databits
 
USART_Enable_TypeDef enable
 
bool mvdis
 
USART_OVS_TypeDef oversampling
 
USART_Parity_TypeDef parity
 
USART_PRS_Channel_t prsRxCh
 
bool prsRxEnable
 
uint32_t refFreq
 
USART_Stopbits_TypeDef stopbits
 

Field Documentation

bool USART_InitAsync_TypeDef::autoCsEnable

Auto CS enabling.

Definition at line 320 of file em_usart.h.

Referenced by USART_InitAsync().

uint32_t USART_InitAsync_TypeDef::baudrate

Desired baud rate.

Definition at line 293 of file em_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().

USART_Databits_TypeDef USART_InitAsync_TypeDef::databits

Number of data bits in frame. Notice that UART modules only support 8 or 9 data bits.

Definition at line 300 of file em_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().

USART_Enable_TypeDef USART_InitAsync_TypeDef::enable

Specifies whether TX and/or RX is enabled when initialization is completed.

Definition at line 284 of file em_usart.h.

Referenced by RETARGET_SerialInit(), UARTDRV_InitUart(), and USART_InitAsync().

bool USART_InitAsync_TypeDef::mvdis

Majority Vote Disable for 16x, 8x and 6x oversampling modes.

Definition at line 310 of file em_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().

USART_OVS_TypeDef USART_InitAsync_TypeDef::oversampling

Oversampling used.

Definition at line 296 of file em_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().

USART_Parity_TypeDef USART_InitAsync_TypeDef::parity

Parity mode to use.

Definition at line 303 of file em_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().

USART_PRS_Channel_t USART_InitAsync_TypeDef::prsRxCh

Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).

Definition at line 316 of file em_usart.h.

Referenced by USART_InitAsync().

bool USART_InitAsync_TypeDef::prsRxEnable

Enable USART Rx via PRS.

Definition at line 313 of file em_usart.h.

Referenced by USART_InitAsync().

uint32_t USART_InitAsync_TypeDef::refFreq

USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.

Definition at line 290 of file em_usart.h.

Referenced by USART_InitAsync().

USART_Stopbits_TypeDef USART_InitAsync_TypeDef::stopbits

Number of stop bits to use.

Definition at line 306 of file em_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/em_usart.h