NUMBER_TypeDef Struct ReferenceKit Drivers > SegmentLcd

Defines segment COM and BIT fields numeric display.

Definition at line 91 of file segmentlcd.c.

Data Fields

uint8_t bit [7]
 
uint8_t com [7]
 

Field Documentation

uint8_t NUMBER_TypeDef::bit[7]

LCD bit number

Definition at line 93 of file segmentlcd.c.

Referenced by SegmentLCD_Number(), and SegmentLCD_UnsignedHex().

uint8_t NUMBER_TypeDef::com[7]

LCD COM line (for multiplexing)

Definition at line 92 of file segmentlcd.c.

Referenced by SegmentLCD_Number(), and SegmentLCD_UnsignedHex().


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/segmentlcd.c