DAC_InitChannel_TypeDef Struct ReferenceEMLIB > DAC

DAC channel initialization structure.

Definition at line 185 of file em_dac.h.

#include <em_dac.h>

Data Fields

bool enable
 
bool prsEnable
 
DAC_PRSSEL_TypeDef prsSel
 
bool refreshEnable
 

Field Documentation

bool DAC_InitChannel_TypeDef::enable

Enable channel.

Definition at line 187 of file em_dac.h.

Referenced by DAC_InitChannel().

bool DAC_InitChannel_TypeDef::prsEnable

Peripheral reflex system trigger enable. If false, channel is triggered by writing to CHnDATA.

Definition at line 193 of file em_dac.h.

Referenced by DAC_InitChannel().

DAC_PRSSEL_TypeDef DAC_InitChannel_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 206 of file em_dac.h.

Referenced by DAC_InitChannel().

bool DAC_InitChannel_TypeDef::refreshEnable

Enable/disable automatic refresh of channel. Refresh interval must be defined in common control initialization, see DAC_Init() for more information.

Definition at line 200 of file em_dac.h.

Referenced by DAC_InitChannel().


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/em_dac.h