ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC

Single conversion initialization structure.

Definition at line 964 of file em_adc.h .

#include < em_adc.h >

Data Fields

ADC_AcqTime_TypeDef acqTime
bool diff
ADC_SingleInput_TypeDef input
bool leftAdjust
bool prsEnable
ADC_PRSSEL_TypeDef prsSel
ADC_Ref_TypeDef reference
bool rep
ADC_Res_TypeDef resolution

Field Documentation

ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime

Acquisition time (in ADC clock cycles).

Definition at line 972 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and adcInit() .

bool ADC_InitSingle_TypeDef::diff

Select if single-ended or differential input.

Definition at line 1003 of file em_adc.h .

Referenced by ADC_InitSingle() .

ADC_SingleInput_TypeDef ADC_InitSingle_TypeDef::input

Sample input selection, use single-ended or differential input according to setting of diff .

Definition at line 988 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .

bool ADC_InitSingle_TypeDef::leftAdjust

Select if left adjustment should be done.

Definition at line 1009 of file em_adc.h .

Referenced by ADC_InitSingle() .

bool ADC_InitSingle_TypeDef::prsEnable

Peripheral reflex system trigger enable.

Definition at line 1006 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 969 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference

Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.

Definition at line 978 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , adcInit() , and TOUCH_Init() .

bool ADC_InitSingle_TypeDef::rep

Select if continuous conversion until explicit stop.

Definition at line 1012 of file em_adc.h .

Referenced by ADC_InitSingle() .

ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution

Sample resolution.

Definition at line 981 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/ em_adc.h