IDAC
Detailed Description
Current Digital-to-Analog Converter (IDAC) Peripheral API.
IDAC can source or sink a configurable constant current, which can be output on, or sinked from pin or ADC. Current is configurable with several ranges of various step sizes. IDAC can be used with PRS and can operate down to EM3.
The following steps are necessary for basic operation:
Clock enable:
Initialize peripheral with default settings and modify selected fields, such as output select:
Set output:
| Data Structures | |
| struct | IDAC_Init_TypeDef | 
| Macros | |
| #define | IDAC_INIT_DEFAULT | 
| Enumerations | |
| enum | IDAC_OutMode_TypeDef
         
         { idacOutputPin = IDAC_CTRL_OUTMODE_PIN, idacOutputADC = IDAC_CTRL_OUTMODE_ADC } | 
| enum | IDAC_PRSSEL_TypeDef
         
         { idacPRSSELCh0 = IDAC_CTRL_PRSSEL_PRSCH0, idacPRSSELCh1 = IDAC_CTRL_PRSSEL_PRSCH1, idacPRSSELCh2 = IDAC_CTRL_PRSSEL_PRSCH2, idacPRSSELCh3 = IDAC_CTRL_PRSSEL_PRSCH3, idacPRSSELCh4 = IDAC_CTRL_PRSSEL_PRSCH4, idacPRSSELCh5 = IDAC_CTRL_PRSSEL_PRSCH5 } | 
| enum | IDAC_Range_TypeDef
         
         { idacCurrentRange0 = IDAC_CURPROG_RANGESEL_RANGE0, idacCurrentRange1 = IDAC_CURPROG_RANGESEL_RANGE1, idacCurrentRange2 = IDAC_CURPROG_RANGESEL_RANGE2, idacCurrentRange3 = IDAC_CURPROG_RANGESEL_RANGE3 } | 
| Functions | |
| void | IDAC_Enable (IDAC_TypeDef *idac, bool enable) | 
| Enable/disable IDAC. | |
| void | IDAC_Init (IDAC_TypeDef *idac, const IDAC_Init_TypeDef *init) | 
| Initialize IDAC. | |
| void | IDAC_MinimalOutputTransitionMode (IDAC_TypeDef *idac, bool enable) | 
| Enable/disable Minimal Output Transition mode. | |
| void | IDAC_OutEnable (IDAC_TypeDef *idac, bool enable) | 
| Enable/disable the IDAC OUT pin. | |
| void | IDAC_RangeSet (IDAC_TypeDef *idac, const IDAC_Range_TypeDef range) | 
| Set the current range of the IDAC output. | |
| void | IDAC_Reset (IDAC_TypeDef *idac) | 
| Reset IDAC to the same state that it was in after a hardware reset. | |
| void | IDAC_StepSet (IDAC_TypeDef *idac, const uint32_t step) | 
| Set the current step of the IDAC output. | |
Macro Definition Documentation
| #define IDAC_INIT_DEFAULT | 
Default configuration for IDAC initialization structure.
        Definition at line
        
         191
        
        of file
        
         em_idac.h
        
        .
       
Enumeration Type Documentation
| enum IDAC_OutMode_TypeDef | 
| enum IDAC_PRSSEL_TypeDef | 
Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.
| Enumerator | |
|---|---|
| idacPRSSELCh0 | PRS channel 0. | 
| idacPRSSELCh1 | PRS channel 1. | 
| idacPRSSELCh2 | PRS channel 2. | 
| idacPRSSELCh3 | PRS channel 3. | 
| idacPRSSELCh4 | PRS channel 4. | 
| idacPRSSELCh5 | PRS channel 5. | 
        Definition at line
        
         133
        
        of file
        
         em_idac.h
        
        .
       
| enum IDAC_Range_TypeDef | 
Function Documentation
| void IDAC_Enable | ( | IDAC_TypeDef * | 
            idac,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable/disable IDAC.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. [in] enableTrue to enable IDAC, false to disable. 
        Definition at line
        
         113
        
        of file
        
         em_idac.c
        
        .
       
References BUS_RegBitWrite() .
| void IDAC_Init | ( | IDAC_TypeDef * | 
            idac,
            | 
| const IDAC_Init_TypeDef * | 
            init
            | ||
| ) | 
Initialize IDAC.
Initializes IDAC according to the initialization structure parameter and sets the default calibration value stored in the DEVINFO structure.
- Note
- This function will disable IDAC prior to configuration.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. [in] initA pointer to the IDAC initialization structure. 
        Definition at line
        
         76
        
        of file
        
         em_idac.c
        
        .
       
References IDAC_Init_TypeDef::enable , IDAC_Init_TypeDef::outMode , IDAC_Init_TypeDef::prsEnable , IDAC_Init_TypeDef::prsSel , and IDAC_Init_TypeDef::sinkEnable .
| void IDAC_MinimalOutputTransitionMode | ( | IDAC_TypeDef * | 
            idac,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable/disable Minimal Output Transition mode.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. [in] enableTrue to enable Minimal Output Transition mode, false to disable. 
        Definition at line
        
         164
        
        of file
        
         em_idac.c
        
        .
       
References BUS_RegBitWrite() .
| void IDAC_OutEnable | ( | IDAC_TypeDef * | 
            idac,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable/disable the IDAC OUT pin.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. [in] enableTrue to enable the IDAC OUT pin, false to disable. 
        Definition at line
        
         329
        
        of file
        
         em_idac.c
        
        .
       
References BUS_RegBitWrite() .
| void IDAC_RangeSet | ( | IDAC_TypeDef * | 
            idac,
            | 
| const IDAC_Range_TypeDef | 
            range
            | ||
| ) | 
Set the current range of the IDAC output.
This function sets the current range of the IDAC output. The function also updates the IDAC calibration register (IDAC_CAL) with the default calibration value from DEVINFO (factory calibration) corresponding to the specified range.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. [in] rangeThe current range value. 
        Definition at line
        
         186
        
        of file
        
         em_idac.c
        
        .
       
References idacCurrentRange0 , idacCurrentRange1 , idacCurrentRange2 , and idacCurrentRange3 .
| void IDAC_Reset | ( | IDAC_TypeDef * | 
            idac
            | ) | 
Reset IDAC to the same state that it was in after a hardware reset.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. 
        Definition at line
        
         126
        
        of file
        
         em_idac.c
        
        .
       
| void IDAC_StepSet | ( | IDAC_TypeDef * | 
            idac,
            | 
| const uint32_t | 
            step
            | ||
| ) | 
Set the current step of the IDAC output.
- Parameters
- 
         [in] idacA pointer to the IDAC peripheral register block. [in] stepA step value for the IDAC output. A valid range is 0-31. 
        Definition at line
        
         306
        
        of file
        
         em_idac.c
        
        .