Status Codes

Macros

#define SL_STATUS_ABORT   ((sl_status_t)0x0006)
 Operation aborted.
 
#define SL_STATUS_ALLOCATION_FAILED   ((sl_status_t)0x0019)
 Generic allocation error.
 
#define SL_STATUS_ALREADY_EXISTS   ((sl_status_t)0x002E)
 Item already exists.
 
#define SL_STATUS_ALREADY_INITIALIZED   ((sl_status_t)0x0012)
 Module has already been initialized.
 
#define SL_STATUS_BLUETOOTH_ATT_SPACE   ((sl_status_t)0x1100)
 
#define SL_STATUS_BLUETOOTH_CTRL_SPACE   ((sl_status_t)0x1000)
 
#define SL_STATUS_BLUETOOTH_MESH_FOUNDATION_SPACE   ((sl_status_t)0x1300)
 
#define SL_STATUS_BLUETOOTH_MESH_SPACE   ((sl_status_t)0x0500)
 
#define SL_STATUS_BLUETOOTH_SMP_SPACE   ((sl_status_t)0x1200)
 
#define SL_STATUS_BLUETOOTH_SPACE   ((sl_status_t)0x0400)
 
#define SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERROR   ((sl_status_t)0x041E)
 Encrypion/decryption operation failed.
 
#define SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITY   ((sl_status_t)0x041D)
 Mismatched or insufficient security level.
 
#define SL_STATUS_BT_ATT_APPLICATION   ((sl_status_t)0x1180)
 When this is returned in a BGAPI response, the application tried to read or write the value of a user attribute from the GATT databa.
 
#define SL_STATUS_BT_ATT_ATT_NOT_FOUND   ((sl_status_t)0x110A)
 No attribute found within the given attribute handle range.
 
#define SL_STATUS_BT_ATT_ATT_NOT_LONG   ((sl_status_t)0x110B)
 The attribute cannot be read or written using the Read Blob Request.
 
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATION   ((sl_status_t)0x1105)
 The attribute requires authentication before it can be read or written.
 
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATION   ((sl_status_t)0x1108)
 The attribute requires authorization before it can be read or written.
 
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZE   ((sl_status_t)0x110C)
 The Encryption Key Size used for encrypting this link is insufficient.
 
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTION   ((sl_status_t)0x110F)
 The attribute requires encryption before it can be read or written.
 
#define SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCES   ((sl_status_t)0x1111)
 Insufficient Resources to complete the request.
 
#define SL_STATUS_BT_ATT_INVALID_ATT_LENGTH   ((sl_status_t)0x110D)
 The attribute value length is invalid for the operation.
 
#define SL_STATUS_BT_ATT_INVALID_HANDLE   ((sl_status_t)0x1101)
 The attribute handle given was not valid on this server.
 
#define SL_STATUS_BT_ATT_INVALID_OFFSET   ((sl_status_t)0x1107)
 Offset specified was past the end of the attribute.
 
#define SL_STATUS_BT_ATT_INVALID_PDU   ((sl_status_t)0x1104)
 The attribute PDU was invalid.
 
#define SL_STATUS_BT_ATT_OUT_OF_SYNC   ((sl_status_t)0x1112)
 The server requests the client to rediscover the database.
 
#define SL_STATUS_BT_ATT_PREPARE_QUEUE_FULL   ((sl_status_t)0x1109)
 Too many prepare writes have been queueud.
 
#define SL_STATUS_BT_ATT_READ_NOT_PERMITTED   ((sl_status_t)0x1102)
 The attribute cannot be read.
 
#define SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTED   ((sl_status_t)0x1106)
 Attribute Server does not support the request received from the client.
 
#define SL_STATUS_BT_ATT_UNLIKELY_ERROR   ((sl_status_t)0x110E)
 The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested.
 
#define SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPE   ((sl_status_t)0x1110)
 The attribute type is not a supported grouping attribute as defined by a higher layer specification.
 
#define SL_STATUS_BT_ATT_VALUE_NOT_ALLOWED   ((sl_status_t)0x1113)
 The attribute parameter value was not allowed.
 
#define SL_STATUS_BT_ATT_WRITE_NOT_PERMITTED   ((sl_status_t)0x1103)
 The attribute cannot be written.
 
#define SL_STATUS_BT_CRYPTO   ((sl_status_t)0x0407)
 Error using crypto functions.
 
#define SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTS   ((sl_status_t)0x100B)
 The ACL Connection Already Exists error code indicates that an attempt to create a new ACL Connection to a device when there is already a connection to this device.
 
#define SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT   ((sl_status_t)0x103C)
 Ddvertising for a fixed duration completed or, for directed advertising, that advertising completed without a connection being created.
 
#define SL_STATUS_BT_CTRL_AUTHENTICATION_FAILURE   ((sl_status_t)0x1005)
 Pairing or authentication failed due to incorrect results in the pairing or authentication procedure. This could be due to an incorrect PIN or Link Key.
 
#define SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTED   ((sl_status_t)0x102E)
 The Controller cannot perform channel assessment because it is not supported.
 
#define SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGING   ((sl_status_t)0x1040)
 The master, at this time, is unable to make a coarse adjustment to the piconet clock, using the supplied parameters. Instead the master will attempt to move the clock using clock dragging.
 
#define SL_STATUS_BT_CTRL_COMMAND_DISALLOWED   ((sl_status_t)0x100C)
 Command requested cannot be executed because the Controller is in a state where it cannot process this command at this time.
 
#define SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDED   ((sl_status_t)0x1010)
 The Connection Accept Timeout has been exceeded for this connection attempt.
 
#define SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHED   ((sl_status_t)0x103E)
 LL initiated a connection but the connection has failed to be established. Controller did not receive any packets from remote end.
 
#define SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDED   ((sl_status_t)0x1009)
 Controller is at limit of connections it can support.
 
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCES   ((sl_status_t)0x100D)
 The Connection Rejected Due To Limited Resources error code indicates that an incoming connection was rejected due to limited resources.
 
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUND   ((sl_status_t)0x1039)
 The Controller could not calculate an appropriate value for the Channel selection operation.
 
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONS   ((sl_status_t)0x100E)
 The Connection Rejected Due To Security Reasons error code indicates that a connection was rejected due to security requirements not being fulfilled, like authentication or pairing.
 
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDR   ((sl_status_t)0x100F)
 The Connection was rejected because this device does not accept the BD_ADDR. This may be because the device will only accept connections from specific BD_ADDRs.
 
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOST   ((sl_status_t)0x1016)
 Local device terminated the connection.
 
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE   ((sl_status_t)0x103D)
 Connection was terminated because the Message Integrity Check (MIC) failed on a received packet.
 
#define SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT   ((sl_status_t)0x1008)
 Link supervision timeout has expired.
 
#define SL_STATUS_BT_CTRL_CONTROLLER_BUSY   ((sl_status_t)0x103A)
 Operation was rejected because the controller is busy and unable to process the request.
 
#define SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISION   ((sl_status_t)0x102A)
 LMP transaction was started that collides with an ongoing transaction.
 
#define SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLE   ((sl_status_t)0x1025)
 The requested encryption mode is not acceptable at this time.
 
#define SL_STATUS_BT_CTRL_HOST_BUSY_PAIRING   ((sl_status_t)0x1038)
 The Host is busy with another pairing operation and unable to support the requested pairing. The receiving device should retry pairing again later.
 
#define SL_STATUS_BT_CTRL_INSTANT_PASSED   ((sl_status_t)0x1028)
 LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed.
 
#define SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY   ((sl_status_t)0x102F)
 The HCI command or LMP PDU sent is only possible on an encrypted link.
 
#define SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS   ((sl_status_t)0x1012)
 Command contained invalid parameters.
 
#define SL_STATUS_BT_CTRL_LIMIT_REACHED   ((sl_status_t)0x1043)
 Number of operations requested has been reached and has indicated the completion of the activity (e.g., advertising or scanning).
 
#define SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGED   ((sl_status_t)0x1026)
 Link key cannot be changed because a fixed unit key is being used.
 
#define SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISION   ((sl_status_t)0x1023)
 LL procedure has collided with the same transaction or procedure that is already in progress.
 
#define SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUT   ((sl_status_t)0x1022)
 Connection terminated due to link-layer procedure timeout.
 
#define SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILED   ((sl_status_t)0x103F)
 The MAC of the 802.11 AMP was requested to connect to a peer, but the connection failed.
 
#define SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDED   ((sl_status_t)0x1007)
 Controller is out of memory.
 
#define SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOST   ((sl_status_t)0x1044)
 A request to the Controller issued by the Host and still pending was successfully canceled.
 
#define SL_STATUS_BT_CTRL_PACKET_TOO_LONG   ((sl_status_t)0x1045)
 An attempt was made to send or receive a packet that exceeds the maximum allowed packet l.
 
#define SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWED   ((sl_status_t)0x1018)
 The device does not allow pairing. This can be for example, when a device only allows pairing during a certain time window after some user input allows pairing.
 
#define SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED   ((sl_status_t)0x1029)
 It was not possible to pair as a unit key was requested and it is not supported.
 
#define SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGE   ((sl_status_t)0x1030)
 A parameter value requested is outside the mandatory range of parameters for the given HCI command or LMP PDU.
 
#define SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSING   ((sl_status_t)0x1006)
 Pairing failed because of missing PIN, or authentication failed because of missing Key.
 
#define SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCES   ((sl_status_t)0x1014)
 The remote device terminated the connection because of low resources.
 
#define SL_STATUS_BT_CTRL_REMOTE_POWERING_OFF   ((sl_status_t)0x1015)
 Remote Device Terminated Connection due to Power Off.
 
#define SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATED   ((sl_status_t)0x1013)
 User on the remote device terminated the connection.
 
#define SL_STATUS_BT_CTRL_REPEATED_ATTEMPTS   ((sl_status_t)0x1017)
 The Controller is disallowing an authentication or pairing procedure because too little time has elapsed since the last authentication or pairing attempt failed.
 
#define SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST   ((sl_status_t)0x1037)
 The IO capabilities request or response was rejected because the sending Host does not support Secure Simple Pairing even though the receiving Link Manager does.
 
#define SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTIONTION_LIMIT_EXCEEDED   ((sl_status_t)0x100A)
 The Synchronous Connection Limit to a Device Exceeded error code indicates that the Controller has reached the limit to the number of synchronous connections that can be achieved to a device.
 
#define SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVAL   ((sl_status_t)0x103B)
 Remote device terminated the connection because of an unacceptable connection interval.
 
#define SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIER   ((sl_status_t)0x1042)
 A command was sent from the Host that should identify an Advertising or Sync handle, but the Advertising or Sync handle does not exist.
 
#define SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIER   ((sl_status_t)0x1002)
 Connection does not exist, or connection open request was cancelled.
 
#define SL_STATUS_BT_CTRL_UNSPECIFIED_ERROR   ((sl_status_t)0x101F)
 No other error code specified is appropriate to use.
 
#define SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE   ((sl_status_t)0x1011)
 A feature or parameter value in the HCI command is not supported.
 
#define SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE   ((sl_status_t)0x101A)
 The remote device does not support the feature associated with the issued command.
 
#define SL_STATUS_BT_DATA_CORRUPTED   ((sl_status_t)0x0408)
 Data was corrupted.
 
#define SL_STATUS_BT_HARDWARE   ((sl_status_t)0x0404)
 Hardware failure.
 
#define SL_STATUS_BT_INVALID_MODULE_ACTION   ((sl_status_t)0x040B)
 Bluetooth cannot be used on this hardware.
 
#define SL_STATUS_BT_INVALID_SYNC_HANDLE   ((sl_status_t)0x040A)
 Invalid periodic advertising sync handle.
 
#define SL_STATUS_BT_L2CAP_CID_NOT_EXIST   ((sl_status_t)0x040F)
 Returned when local host did not find a connection-oriented channel with given destination CID.
 
#define SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUT   ((sl_status_t)0x0415)
 Returned when connection-oriented channel has not received connection response message within maximum timeout.
 
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWED   ((sl_status_t)0x0413)
 Returned when connection-oriented channel disconnected due to remote end send flow control credits exceed 65535.
 
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATED   ((sl_status_t)0x0412)
 Returned when connection-oriented channel disconnected due to remote end send data even without credit.
 
#define SL_STATUS_BT_L2CAP_INVALID_CID   ((sl_status_t)0x0416)
 Returned when local host received a connection-oriented channel connection response with an invalid destination CID.
 
#define SL_STATUS_BT_L2CAP_LE_DISCONNECTED   ((sl_status_t)0x0410)
 Returned when connection-oriented channel disconnected due to LE connection is dropped.
 
#define SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTED   ((sl_status_t)0x040E)
 Returned when local host disconnect the connection-oriented channel by sending disconnection request.
 
#define SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDIT   ((sl_status_t)0x0414)
 Returned when connection-oriented channel has run out of flow control credit and local application still trying to send data.
 
#define SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTED   ((sl_status_t)0x040D)
 Returned when remote disconnects the connection-oriented channel by sending disconnection request.
 
#define SL_STATUS_BT_L2CAP_WRONG_STATE   ((sl_status_t)0x0417)
 Returned when local host application tries to send a command which is not suitable for L2CAP channel's current state.
 
#define SL_STATUS_BT_MESH_ADDRESS_ALREADY_USED   ((sl_status_t)0x0513)
 Returned when trying to assign an address that is used by one of the devices in the Device Database, or by the Provisioner itself.
 
#define SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLE   ((sl_status_t)0x0512)
 Returned when trying to reuse an address of a previously deleted device before an IV Index Update has been executed.
 
#define SL_STATUS_BT_MESH_ALREADY_EXISTS   ((sl_status_t)0x0501)
 Returned when trying to add a key or some other unique resource with an ID which already exists.
 
#define SL_STATUS_BT_MESH_ALREADY_INITIALIZED   ((sl_status_t)0x0506)
 An attempt was made to initialize a subsystem that was already initialized.
 
#define SL_STATUS_BT_MESH_DOES_NOT_EXIST   ((sl_status_t)0x0502)
 Returned when trying to manipulate a key or some other resource with an ID which does not exist.
 
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BIND   ((sl_status_t)0x130D)
 Returned when the requested bind operation cannot be performed due to general constraints.
 
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVE   ((sl_status_t)0x130C)
 Returned when the requested delete operation cannot be performed due to general constraints.
 
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SET   ((sl_status_t)0x130F)
 Returned when the requested state cannot be set.
 
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATE   ((sl_status_t)0x130B)
 Returned when the requested update operation cannot be performed due to general constraints.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCES   ((sl_status_t)0x1305)
 Returned when The node cannot serve the request due to insufficient resources.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESS   ((sl_status_t)0x1301)
 Returned when address in request was not valid.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEY   ((sl_status_t)0x1303)
 Returned when the key identified by AppKeyIndex is not stored in the node.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDING   ((sl_status_t)0x1311)
 Returned when the NetKeyIndex and AppKeyIndex combination is not valid for a Config AppKey Update.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODEL   ((sl_status_t)0x1302)
 Returned when model identified is not found for a given element.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEY   ((sl_status_t)0x1304)
 Returned when the key identified by NetKeyIndex is not stored in the node.
 
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMS   ((sl_status_t)0x1307)
 Returned when the model does not support the publish mechanism.
 
#define SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTS   ((sl_status_t)0x1306)
 Returned when the key identified is already stored in the node and the new NetKey value is different.
 
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODEL   ((sl_status_t)0x1308)
 Returned when the model does not support the subscribe mechanism.
 
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTED   ((sl_status_t)0x130A)
 Returned when requested setting is not supported.
 
#define SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILURE   ((sl_status_t)0x1309)
 Returned when storing of the requested parameters failed.
 
#define SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLE   ((sl_status_t)0x130E)
 Returned when The node cannot start advertising with Node Identity or Proxy since the maximum number of parallel advertising is reached.
 
#define SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIED   ((sl_status_t)0x1310)
 Returned when an unspecified error took place.
 
#define SL_STATUS_BT_MESH_INVALID_ADDRESS   ((sl_status_t)0x0504)
 Returned when trying to use a reserved address or add a "pre-provisioned" device using an address already used by some other device.
 
#define SL_STATUS_BT_MESH_LIMIT_REACHED   ((sl_status_t)0x0503)
 Returned when an operation cannot be executed because a pre-configured limit for keys, key bindings, elements, models, virtual addresses, provisioned devices, or provisioning sessions is reached.
 
#define SL_STATUS_BT_MESH_MALFORMED_DATA   ((sl_status_t)0x0505)
 In a BGAPI response, the user supplied malformed data; in a BGAPI event, the remote end responded with malformed or unrecognized data.
 
#define SL_STATUS_BT_MESH_NO_FRIEND_OFFER   ((sl_status_t)0x0508)
 Returned when trying to establish a friendship as a Low Power Node, but no acceptable friend offer message was received.
 
#define SL_STATUS_BT_MESH_NOT_INITIALIZED   ((sl_status_t)0x0507)
 An attempt was made to use a subsystem that wasn't initialized yet. Call the subsystem's init function first.
 
#define SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDR   ((sl_status_t)0x0511)
 Device could not assign unicast addresses to all of its elements.
 
#define SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILED   ((sl_status_t)0x050D)
 The computed confirmation value did not match the expected value.
 
#define SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILED   ((sl_status_t)0x050F)
 The provisioning data block could not be decrypted.
 
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU   ((sl_status_t)0x050A)
 An unrecognized provisioning PDU was received.
 
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMAT   ((sl_status_t)0x050B)
 A provisioning PDU with wrong length or containing field values that are out of bounds was received.
 
#define SL_STATUS_BT_MESH_PROV_LINK_CLOSED   ((sl_status_t)0x0509)
 Provisioning link was unexpectedly closed before provisioning was complete.
 
#define SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCES   ((sl_status_t)0x050E)
 Provisioning could not be continued due to insufficient resources.
 
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERROR   ((sl_status_t)0x0510)
 An unexpected error happened during provisioning.
 
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDU   ((sl_status_t)0x050C)
 An unexpected (out of sequence) provisioning PDU was received.
 
#define SL_STATUS_BT_NO_BONDING   ((sl_status_t)0x0406)
 The bonding does not exist.
 
#define SL_STATUS_BT_OUT_OF_BONDS   ((sl_status_t)0x0402)
 Bonding procedure can't be started because device has no space left for bond.
 
#define SL_STATUS_BT_PS_KEY_NOT_FOUND   ((sl_status_t)0x041C)
 PS key not found.
 
#define SL_STATUS_BT_PS_STORE_FULL   ((sl_status_t)0x041B)
 Flash reserved for PS store is full.
 
#define SL_STATUS_BT_RADIO   ((sl_status_t)0x040C)
 Error received from radio.
 
#define SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTS   ((sl_status_t)0x1203)
 The pairing procedure cannot be performed as authentication requirements cannot be met due to IO capabilities of one or both devices.
 
#define SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESS   ((sl_status_t)0x120D)
 Indicates that the pairing over the LE transport failed due to a Pairing Request sent over the BR/EDR transport in process.
 
#define SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTED   ((sl_status_t)0x1207)
 The SMP command received is not supported on this device.
 
#define SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILED   ((sl_status_t)0x1204)
 The confirm value does not match the calculated compare value.
 
#define SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWED   ((sl_status_t)0x120E)
 Indicates that the BR/EDR Link Key generated on the BR/EDR transport cannot be used to derive and distribute keys for the LE transport.
 
#define SL_STATUS_BT_SMP_DHKEY_CHECK_FAILED   ((sl_status_t)0x120B)
 Indicates to the remote device that the DHKey Check value received doesn't match the one calculated by the local device.
 
#define SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZE   ((sl_status_t)0x1206)
 The resultant encryption key size is insufficient for the security requirements of this device.
 
#define SL_STATUS_BT_SMP_INVALID_PARAMETERS   ((sl_status_t)0x120A)
 The Invalid Parameters error code indicates: the command length is invalid or a parameter is outside of the specified range.
 
#define SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILED   ((sl_status_t)0x120C)
 Indicates that the confirm values in the numeric comparison protocol do not match.
 
#define SL_STATUS_BT_SMP_OOB_NOT_AVAILABLE   ((sl_status_t)0x1202)
 Out of Band data is not available for authentication.
 
#define SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTED   ((sl_status_t)0x1205)
 Pairing is not supported by the device.
 
#define SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILED   ((sl_status_t)0x1201)
 The user input of passkey failed, for example, the user cancelled the operation.
 
#define SL_STATUS_BT_SMP_REPEATED_ATTEMPTS   ((sl_status_t)0x1209)
 Pairing or authentication procedure is disallowed because too little time has elapsed since last pairing request or security request.
 
#define SL_STATUS_BT_SMP_UNSPECIFIED_REASON   ((sl_status_t)0x1208)
 Pairing failed due to an unspecified reason.
 
#define SL_STATUS_BT_UNSPECIFIED   ((sl_status_t)0x0403)
 Unspecified error.
 
#define SL_STATUS_BUS_ERROR   ((sl_status_t)0x004B)
 Bus error, e.g. invalid DMA address.
 
#define SL_STATUS_BUSY   ((sl_status_t)0x0004)
 Module is busy and cannot carry out requested operation.
 
#define SL_STATUS_CAN_CANOPEN_SPACE   ((sl_status_t)0x0600)
 
#define SL_STATUS_CLI_STORAGE_NVM_OPEN_ERROR   ((sl_status_t)0x0045)
 Error in open NVM.
 
#define SL_STATUS_COMMAND_INCOMPLETE   ((sl_status_t)0x004A)
 Data received does not form a complete command.
 
#define SL_STATUS_COMMAND_IS_INVALID   ((sl_status_t)0x0048)
 Command was not recognized.
 
#define SL_STATUS_COMMAND_TOO_LONG   ((sl_status_t)0x0049)
 Command maximum length exceeded.
 
#define SL_STATUS_CONNECT_SPACE   ((sl_status_t)0x0700)
 
#define SL_STATUS_DELETED   ((sl_status_t)0x0013)
 Object/construct has been deleted.
 
#define SL_STATUS_EEPROM_MFG_VERSION_MISMATCH   ((sl_status_t)0x0039)
 
#define SL_STATUS_EEPROM_STACK_VERSION_MISMATCH   ((sl_status_t)0x003A)
 
#define SL_STATUS_EMPTY   ((sl_status_t)0x001B)
 Item/list/queue is empty.
 
#define SL_STATUS_FAIL   ((sl_status_t)0x0001)
 Generic error.
 
#define SL_STATUS_FLASH_ERASE_FAILED   ((sl_status_t)0x003E)
 Flash erase failed.
 
#define SL_STATUS_FLASH_PROGRAM_FAILED   ((sl_status_t)0x003D)
 Flash programming failed.
 
#define SL_STATUS_FLASH_VERIFY_FAILED   ((sl_status_t)0x003C)
 Flash verification failed.
 
#define SL_STATUS_FLASH_WRITE_INHIBITED   ((sl_status_t)0x003B)
 Flash write is inhibited.
 
#define SL_STATUS_FULL   ((sl_status_t)0x001C)
 Item/list/queue is full.
 
#define SL_STATUS_GECKO_OS_1_SPACE   ((sl_status_t)0x0E00)
 
#define SL_STATUS_GECKO_OS_2_SPACE   ((sl_status_t)0x0F00)
 
#define SL_STATUS_GENERIC_SPACE   ((sl_status_t)0x0000)
 
#define SL_STATUS_HARDWARE_SPACE   ((sl_status_t)0x0300)
 
#define SL_STATUS_HAS_OVERFLOWED   ((sl_status_t)0x001E)
 Item/list/queue has been overflowed.
 
#define SL_STATUS_IDLE   ((sl_status_t)0x000A)
 Operation/module is Idle, cannot carry requested operation.
 
#define SL_STATUS_IN_PROGRESS   ((sl_status_t)0x0005)
 Operation is in progress and not yet complete (pass or fail).
 
#define SL_STATUS_INITIALIZATION   ((sl_status_t)0x0010)
 Initialization failed.
 
#define SL_STATUS_INVALID_CONFIGURATION   ((sl_status_t)0x0023)
 Invalid configuration provided.
 
#define SL_STATUS_INVALID_COUNT   ((sl_status_t)0x002B)
 Invalid count.
 
#define SL_STATUS_INVALID_CREDENTIALS   ((sl_status_t)0x002A)
 Invalid credentials.
 
#define SL_STATUS_INVALID_HANDLE   ((sl_status_t)0x0025)
 Invalid handle.
 
#define SL_STATUS_INVALID_INDEX   ((sl_status_t)0x0027)
 Invalid index.
 
#define SL_STATUS_INVALID_KEY   ((sl_status_t)0x0029)
 Invalid key.
 
#define SL_STATUS_INVALID_MODE   ((sl_status_t)0x0024)
 Invalid mode.
 
#define SL_STATUS_INVALID_PARAMETER   ((sl_status_t)0x0021)
 Generic invalid argument or consequence of invalid argument.
 
#define SL_STATUS_INVALID_RANGE   ((sl_status_t)0x0028)
 Invalid range.
 
#define SL_STATUS_INVALID_SIGNATURE   ((sl_status_t)0x002C)
 Invalid signature / verification failed.
 
#define SL_STATUS_INVALID_STATE   ((sl_status_t)0x0002)
 Generic invalid state error.
 
#define SL_STATUS_INVALID_TYPE   ((sl_status_t)0x0026)
 Invalid type for operation.
 
#define SL_STATUS_IO   ((sl_status_t)0x002F)
 Generic I/O failure.
 
#define SL_STATUS_IO_TIMEOUT   ((sl_status_t)0x0030)
 I/O failure due to timeout.
 
#define SL_STATUS_IS_OWNER   ((sl_status_t)0x0020)
 Already/still owning resource.
 
#define SL_STATUS_IS_WAITING   ((sl_status_t)0x000B)
 Operation cannot be done while construct is waiting.
 
#define SL_STATUS_ISR   ((sl_status_t)0x0014)
 Illegal call from ISR.
 
#define SL_STATUS_MAC_ACK_HEADER_TYPE   ((sl_status_t)0x0043)
 
#define SL_STATUS_MAC_COMMAND_TRANSMIT_FAILURE   ((sl_status_t)0x0044)
 
#define SL_STATUS_MAC_INDIRECT_TIMEOUT   ((sl_status_t)0x0041)
 
#define SL_STATUS_MAC_NO_ACK_RECEIVED   ((sl_status_t)0x0040)
 
#define SL_STATUS_MAC_NO_DATA   ((sl_status_t)0x003F)
 
#define SL_STATUS_MAC_UNKNOWN_HEADER_TYPE   ((sl_status_t)0x0042)
 
#define SL_STATUS_MESSAGE_TOO_LONG   ((sl_status_t)0x0038)
 Message is too long.
 
#define SL_STATUS_NET_SUITE_SPACE   ((sl_status_t)0x0800)
 
#define SL_STATUS_NETWORK_DOWN   ((sl_status_t)0x0016)
 Illegal call because network is down.
 
#define SL_STATUS_NETWORK_UP   ((sl_status_t)0x0015)
 Illegal call because network is up.
 
#define SL_STATUS_NO_BEACONS   ((sl_status_t)0x0018)
 Invalid operation as there are no beacons.
 
#define SL_STATUS_NO_MORE_RESOURCE   ((sl_status_t)0x001A)
 No more resource available to perform the operation.
 
#define SL_STATUS_NONE_WAITING   ((sl_status_t)0x000C)
 No task/construct waiting/pending for that action/event.
 
#define SL_STATUS_NOT_AVAILABLE   ((sl_status_t)0x000E)
 Feature not available due to software configuration.
 
#define SL_STATUS_NOT_FOUND   ((sl_status_t)0x002D)
 Item could not be found.
 
#define SL_STATUS_NOT_INITIALIZED   ((sl_status_t)0x0011)
 Module has not been initialized.
 
#define SL_STATUS_NOT_JOINED   ((sl_status_t)0x0017)
 Failure due to not being joined in a network.
 
#define SL_STATUS_NOT_READY   ((sl_status_t)0x0003)
 Module is not ready for requested operation.
 
#define SL_STATUS_NOT_SUPPORTED   ((sl_status_t)0x000F)
 Feature not supported.
 
#define SL_STATUS_NULL_POINTER   ((sl_status_t)0x0022)
 Invalid null pointer received as argument.
 
#define SL_STATUS_OBJECT_READ   ((sl_status_t)0x0036)
 Failed to read on/via given object.
 
#define SL_STATUS_OBJECT_WRITE   ((sl_status_t)0x0037)
 Failed to write on/via given object.
 
#define SL_STATUS_OK   ((sl_status_t)0x0000)
 No error.
 
#define SL_STATUS_OWNERSHIP   ((sl_status_t)0x001F)
 Generic ownership error.
 
#define SL_STATUS_PERMISSION   ((sl_status_t)0x0008)
 Operation not allowed per permissions.
 
#define SL_STATUS_PLATFORM_1_SPACE   ((sl_status_t)0x0100)
 
#define SL_STATUS_PLATFORM_2_SPACE   ((sl_status_t)0x0200)
 
#define SL_STATUS_RECEIVE   ((sl_status_t)0x0035)
 Generic reception error.
 
#define SL_STATUS_SECURITY_DECRYPT_ERROR   ((sl_status_t)0x0047)
 Decryption failed.
 
#define SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERROR   ((sl_status_t)0x0046)
 Image checksum is not valid.
 
#define SL_STATUS_SPACE_MASK   ((sl_status_t)0xFF00)
 
#define SL_STATUS_SUSPENDED   ((sl_status_t)0x000D)
 Operation cannot be done while construct is suspended.
 
#define SL_STATUS_THREAD_SPACE   ((sl_status_t)0x0900)
 
#define SL_STATUS_TIMEOUT   ((sl_status_t)0x0007)
 Operation timed out.
 
#define SL_STATUS_TRANSMIT   ((sl_status_t)0x0031)
 Generic transmission error.
 
#define SL_STATUS_TRANSMIT_BUSY   ((sl_status_t)0x0034)
 Transmit is busy.
 
#define SL_STATUS_TRANSMIT_INCOMPLETE   ((sl_status_t)0x0033)
 Transmit is incomplete.
 
#define SL_STATUS_TRANSMIT_UNDERFLOW   ((sl_status_t)0x0032)
 Transmit underflowed.
 
#define SL_STATUS_USB_SPACE   ((sl_status_t)0x0A00)
 
#define SL_STATUS_WIFI_CHANNEL_NOT_ALLOWED   ((sl_status_t)0x0B19)
 The request failed due to regulatory limitations.
 
#define SL_STATUS_WIFI_CONNECTION_ABORTED   ((sl_status_t)0x0B1B)
 The connection request was aborted by host.
 
#define SL_STATUS_WIFI_CONNECTION_AUTH_FAILURE   ((sl_status_t)0x0B1E)
 The connection request failed because the WPA handshake did not complete successfully.
 
#define SL_STATUS_WIFI_CONNECTION_REJECTED_BY_AP   ((sl_status_t)0x0B1D)
 The connection request failed because the AP rejected the device.
 
#define SL_STATUS_WIFI_CONNECTION_TIMEOUT   ((sl_status_t)0x0B1C)
 The connection request failed because of a timeout.
 
#define SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT   ((sl_status_t)0x0B02)
 The firmware download took too long.
 
#define SL_STATUS_WIFI_INVALID_KEY   ((sl_status_t)0x0B01)
 Invalid firmware keyset.
 
#define SL_STATUS_WIFI_NO_MATCHING_AP   ((sl_status_t)0x0B1A)
 The connection request failed because no suitable AP was found.
 
#define SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE   ((sl_status_t)0x0B05)
 No Packets waiting to be received.
 
#define SL_STATUS_WIFI_RETRY_EXCEEDED   ((sl_status_t)0x0B1F)
 The request failed because the retry limit was exceeded.
 
#define SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED   ((sl_status_t)0x0B14)
 SecureLink key (re)negotiation failed.
 
#define SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODE   ((sl_status_t)0x0B13)
 The SecureLink MAC key installation failed.
 
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNED   ((sl_status_t)0x0B11)
 The SecureLink MAC key is already installed in OTP.
 
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERROR   ((sl_status_t)0x0B10)
 The SecureLink MAC key was not found.
 
#define SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWED   ((sl_status_t)0x0B12)
 The SecureLink MAC key cannot be installed in RAM.
 
#define SL_STATUS_WIFI_SLEEP_GRANTED   ((sl_status_t)0x0B08)
 The sleep mode is granted.
 
#define SL_STATUS_WIFI_SLEEP_NOT_GRANTED   ((sl_status_t)0x0B09)
 The WFx does not go back to sleep.
 
#define SL_STATUS_WIFI_SPACE   ((sl_status_t)0x0B00)
 
#define SL_STATUS_WIFI_TX_LIFETIME_EXCEEDED   ((sl_status_t)0x0B20)
 The request failed because the MSDU life time was exceeded.
 
#define SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_ID   ((sl_status_t)0x0B03)
 Unknown request ID or wrong interface ID used.
 
#define SL_STATUS_WIFI_WARNING   ((sl_status_t)0x0B04)
 The request is successful but some parameters have been ignored.
 
#define SL_STATUS_WIFI_WRONG_STATE   ((sl_status_t)0x0B18)
 The device is in an inappropriate state to perform the request.
 
#define SL_STATUS_WOULD_BLOCK   ((sl_status_t)0x0009)
 Non-blocking operation would block.
 
#define SL_STATUS_WOULD_OVERFLOW   ((sl_status_t)0x001D)
 Item would overflow.
 
#define SL_STATUS_Z_WAVE_SPACE   ((sl_status_t)0x0D00)
 
#define SL_STATUS_ZIGBEE_SPACE   ((sl_status_t)0x0C00)
 

Typedefs

typedef uint32_t sl_status_t