Initialization structure.
       Definition at line
       
        97
       
       of file
       
        em_leuart.h
       
       .
      
      
       #include <
       
     
        em_leuart.h
       
       >
      
| Data Fields | |
| uint32_t | baudrate | 
| LEUART_Databits_TypeDef | databits | 
| LEUART_Enable_TypeDef | enable | 
| LEUART_Parity_TypeDef | parity | 
| uint32_t | refFreq | 
| LEUART_Stopbits_TypeDef | stopbits | 
Field Documentation
| uint32_t LEUART_Init_TypeDef::baudrate | 
Desired baud rate.
        Definition at line
        
         108
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by BSP_BccInit() , LEUART_Init() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| LEUART_Databits_TypeDef LEUART_Init_TypeDef::databits | 
Number of data bits in frame.
        Definition at line
        
         111
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , and UARTDRV_InitLeuart() .
| LEUART_Enable_TypeDef LEUART_Init_TypeDef::enable | 
Specifies whether TX and/or RX will be enabled when initialization completes.
        Definition at line
        
         99
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| LEUART_Parity_TypeDef LEUART_Init_TypeDef::parity | 
Parity mode to use.
        Definition at line
        
         114
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , and UARTDRV_InitLeuart() .
| uint32_t LEUART_Init_TypeDef::refFreq | 
LEUART reference clock assumed when configuring baud rate setup. Set to 0 if using currently configured reference clock.
        Definition at line
        
         105
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() .
| LEUART_Stopbits_TypeDef LEUART_Init_TypeDef::stopbits | 
Number of stop bits to use.
        Definition at line
        
         117
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , and UARTDRV_InitLeuart() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_leuart.h