Configuration structure for primary or alternate descriptor (not used for scatter-gather DMA cycles).
       Definition at line
       
        201
       
       of file
       
        em_dma.h
       
       .
      
      
       #include <
       
     
        em_dma.h
       
       >
      
| Data Fields | |
| DMA_ArbiterConfig_TypeDef | arbRate | 
| DMA_DataInc_TypeDef | dstInc | 
| uint8_t | hprot | 
| DMA_DataSize_TypeDef | size | 
| DMA_DataInc_TypeDef | srcInc | 
Field Documentation
| DMA_ArbiterConfig_TypeDef DMA_CfgDescr_TypeDef::arbRate | 
Arbitration rate, i.e., number of DMA transfers done before re-arbitration takes place.
        Definition at line
        
         215
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
| DMA_DataInc_TypeDef DMA_CfgDescr_TypeDef::dstInc | 
Destination increment size for each DMA transfer.
        Definition at line
        
         203
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
| uint8_t DMA_CfgDescr_TypeDef::hprot | 
HPROT signal state, refer to reference manual, DMA chapter for further details. Normally set to 0 if protection is not an issue. The following bits are available:
- bit 0 - HPROT[1] control for source read accesses, privileged/non-privileged access.
- bit 3 - HPROT[1] control for destination write accesses, privileged/non-privileged access.
        Definition at line
        
         226
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
| DMA_DataSize_TypeDef DMA_CfgDescr_TypeDef::size | 
| DMA_DataInc_TypeDef DMA_CfgDescr_TypeDef::srcInc | 
Source increment size for each DMA transfer.
        Definition at line
        
         206
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_dma.h