sl_sleeptimer_timer_handle Struct Reference
       Definition at line
       
        63
       
       of file
       
        sl_sleeptimer.h
       
       .
      
| Data Fields | |
| sl_sleeptimer_timer_callback_t | callback | 
| Function to call when timer expires. | |
| void * | callback_data | 
| User data to pass to callback function. | |
| uint32_t | delta | 
| Delay relative to previous element in list. | |
| sl_sleeptimer_timer_handle_t * | next | 
| Pointer to next element in list. | |
| uint16_t | option_flags | 
| Option flags. | |
| uint8_t | priority | 
| Priority of timer. | |
| uint32_t | timeout_periodic | 
| Periodic timeout. | |
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/service/sleeptimer/inc/
       sl_sleeptimer.h