TempSensor
Detailed Description
Driver for DS75 I2C temperature sensor.
| Data Structures | |
| struct | TEMPSENS_Temp_TypeDef | 
| Macros | |
| #define | TEMPSENS_DK_ADDR 0x90 | 
| Enumerations | |
| enum | TEMPSENS_Register_TypeDef
         
         { tempsensRegTemp = 0, tempsensRegConfig = 1, tempsensRegHysteresis = 2, tempsensRegShutdown = 3 } | 
| Functions | |
| void | TEMPSENS_Celsius2Fahrenheit ( TEMPSENS_Temp_TypeDef *temp) | 
| Convert temperature from Celsius to Fahrenheit. | |
| int | TEMPSENS_RegisterGet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t *val) | 
| Read sensor register content. | |
| int | TEMPSENS_RegisterSet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t val) | 
| Write to sensor register. | |
| int | TEMPSENS_TemperatureGet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Temp_TypeDef *temp) | 
| Fetch current temperature from temperature sensor (in Celsius). | |
Macro Definition Documentation
| #define TEMPSENS_DK_ADDR 0x90 | 
I2C device address for temperature sensor on EFM32GG/LG/WG DK
        Definition at line
        
         55
        
        of file
        
         tempsens.h
        
        .
       
Enumeration Type Documentation
Function Documentation
| void TEMPSENS_Celsius2Fahrenheit | ( | TEMPSENS_Temp_TypeDef * | 
            temp
            | ) | 
Convert temperature from Celsius to Fahrenheit.
- Parameters
- 
         [in,out] tempReference to structure to holding temperature in Celsius to convert. Upon return, it has been changed to Fahrenheit. 
        Definition at line
        
         58
        
        of file
        
         tempsens.c
        
        .
       
References TEMPSENS_Temp_TypeDef::f , and TEMPSENS_Temp_TypeDef::i .
| int TEMPSENS_RegisterGet | ( | I2C_TypeDef * | 
            i2c,
            | 
| uint8_t | 
            addr,
            | ||
| TEMPSENS_Register_TypeDef | 
            reg,
            | ||
| uint16_t * | 
            val
            | ||
| ) | 
Read sensor register content.
If reading the temperature register, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Parameters
- 
         [in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] regRegister to read. [out] valReference to place register read. 
- Returns
- Returns 0 if register read, <0 if unable to read register.
        Definition at line
        
         99
        
        of file
        
         tempsens.c
        
        .
       
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_READ , I2CSPM_Transfer() , i2cTransferDone , I2C_TransferSeq_TypeDef::len , and tempsensRegConfig .
Referenced by TEMPSENS_TemperatureGet() .
| int TEMPSENS_RegisterSet | ( | I2C_TypeDef * | 
            i2c,
            | 
| uint8_t | 
            addr,
            | ||
| TEMPSENS_Register_TypeDef | 
            reg,
            | ||
| uint16_t | 
            val
            | ||
| ) | 
Write to sensor register.
- Parameters
- 
         [in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] regRegister to write (temperature register cannot be written). [in] valValue used when writing to register. 
- Returns
- Returns 0 if register written, <0 if unable to write to register.
        Definition at line
        
         156
        
        of file
        
         tempsens.c
        
        .
       
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE , I2CSPM_Transfer() , i2cTransferDone , I2C_TransferSeq_TypeDef::len , tempsensRegConfig , and tempsensRegTemp .
| int TEMPSENS_TemperatureGet | ( | I2C_TypeDef * | 
            i2c,
            | 
| uint8_t | 
            addr,
            | ||
| TEMPSENS_Temp_TypeDef * | 
            temp
            | ||
| ) | 
Fetch current temperature from temperature sensor (in Celsius).
If reading the temperature, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Note
- The sensor on the the DK, STDS75, does not seem to have any check on max temperature limit, ie when exceeding specified max 125 C limit, it will keep increasing 9 bit counter to max representable 9 bit value of 127.5 C and then flip over to negative numbers. There is no limit check in this implementation on such issues.
- Parameters
- 
         [in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [out] tempReference to structure to place temperature (in Celsius). 
- Returns
- Returns 0 if temperature read, <0 if unable to read temperature.
        Definition at line
        
         223
        
        of file
        
         tempsens.c
        
        .
       
References TEMPSENS_Temp_TypeDef::f , TEMPSENS_Temp_TypeDef::i , TEMPSENS_RegisterGet() , and tempsensRegTemp .