VDAC channel initialization structure.
       Definition at line
       
        207
       
       of file
       
        em_vdac.h
       
       .
      
      
       #include <
       
     
        em_vdac.h
       
       >
      
| Data Fields | |
| bool | enable | 
| bool | prsAsync | 
| VDAC_PrsSel_TypeDef | prsSel | 
| bool | sampleOffMode | 
| VDAC_TrigMode_TypeDef | trigMode | 
Field Documentation
| bool VDAC_InitChannel_TypeDef::enable | 
| bool VDAC_InitChannel_TypeDef::prsAsync | 
Treat the PRS signal asynchronously.
        Definition at line
        
         217
        
        of file
        
         em_vdac.h
        
        .
       
Referenced by VDAC_InitChannel() .
| VDAC_PrsSel_TypeDef VDAC_InitChannel_TypeDef::prsSel | 
        Peripheral reflex system trigger selection. Only applicable if
        
         trigMode
        
        is set to
        
         vdacTrigModePrs
        
        or
        
         vdacTrigModeSwPrs
        
        .
       
        Definition at line
        
         214
        
        of file
        
         em_vdac.h
        
        .
       
Referenced by VDAC_InitChannel() .
| bool VDAC_InitChannel_TypeDef::sampleOffMode | 
Set channel conversion mode to sample/shut-off mode. Default is continuous.
        Definition at line
        
         224
        
        of file
        
         em_vdac.h
        
        .
       
Referenced by VDAC_InitChannel() .
| VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode | 
Channel conversion trigger mode.
        Definition at line
        
         220
        
        of file
        
         em_vdac.h
        
        .
       
Referenced by VDAC_InitChannel() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_vdac.h