Modules
      Here is a list of all modules:
     
     | BSP | Board Support Package | 
| API for DKs | |
| API for STKs and WSTKs | |
| Common BSP for all kits | |
| Device Initialization | Device Initialization using HAL configuration | 
| Thunderboard Sense BSP | BSP for Thunderboard Sense and Thunderboard Sense 2 | 
| BAP - Barometric Pressure Sensor | Driver for the Bosch Sensortec BMP280 pressure sensor | 
| BOARD Module for Thunderboard Sense | Board hardware control, configuraton and miscellaneous functions | 
| Power and Interrupt Controller Definitions | Thunderboard Sense 1 Power and Interrupt Controller register and bitfield definitions | 
| BOARD Module for Thunderboard Sense 2 | Board hardware control, configuraton and miscellaneous functions | 
| CCS811 - Indoor Air Quality Sensor | Driver for the Cambridge CMOS Sensors CCS811 gas and indoor air quality sensor | 
| HALL - Hall Effect Sensor | Driver for Hall effect sensor | 
| Si7210 - Hall Effect Sensor | Driver for the Silicon Labs Si7210 Hall effect sensor | 
| ICM20648 - 6-axis Motion Sensor Driver | Driver for the Invensense ICM20648 6-axis motion sensor | 
| IMU - Inertial Measurement Unit | Inertial Measurement Unit driver | 
| MIC - Microphone Driver (ADC) | Driver for the Knowles SPV1840LR5H-B MEMS Microphone | 
| MIC - Microphone Driver (I2S) | Driver for the Invensense ICS-43434 MEMS Microphone | 
| SI1133 - Ambient Light and UV Index Sensor | Driver for the Silicon Labs Si1133 Ambient Light and UV sensor | 
| SI7021 - Relative Humidity and Temperature Sensor | Driver for the Silicon Labs Si7021 I2C Humidity and Temperature Sensor | 
| Utility Functions | Utility functions | 
| Devices | Silicon Laboratories CMSIS-CORE device system headers | 
| EFM32 | |
| EMDRV | Gecko Platform driver library | 
| DMADRV | DMADRV Direct Memory Access Driver | 
| EZRADIODRV | EZR32 EzRadio Peripheral Interface Driver | 
| API_Layer | EzRadio API Layer 
 | 
| COMM_Layer | EzRadio Communication Layer 
 | 
| HAL_Layer | EzRadio HAL Layer 
 | 
| Plugin_System | EzRadio Plugin System Layer, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Auto_ACK_Plugin | Auto acknowledge plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| CRC_Error_Plugin | CRC error plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Direct_Receive_Plugin | Direct receive plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Direct_Transmit_Plugin | Direct transmit plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| PN9_Plugin | Pseudo random transmit plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Plugin_Manager | Plugin manager, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Receive_Plugin | Receive plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Transmit_Plugin | Transmit plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| Unmod_Carrier_Plugin | Unmodulated Carrier plugin, see
          
           Plugin System Layer
          
          for detailed documentation. 
 | 
| GPIOINT | GPIOINT General Purpose Input/Output Interrupt dispatcher | 
| NVM | NVM Non-volatile Memory Wear-Leveling Driver | 
| NVM3 | NVM3 Non-Volatile Memory Management driver | 
| NVM3Hal | NVM3 HAL module | 
| NVM3Lock | NVM3 lock module | 
| RTCDRV | Real-time Clock Driver | 
| SLEEP | Sleep Management Driver | 
| SPIDRV | SPIDRV Serial Peripheral Interface Driver | 
| TEMPDRV | TEMPDRV Temperature Sensor Driver | 
| UARTDRV | UARTDRV Universal Asynchronous Receiver/Transmitter Driver | 
| USTIMER | USTIMER Microsecond Delay Timer Driver | 
| EMLIB | Low-level peripheral library | 
| ACMP | Analog comparator (ACMP) Peripheral API | 
| ADC | Analog to Digital Converter (ADC) Peripheral API | 
| ASSERT | Error checking module | 
| BUS | BUS register and RAM bit/field read/write API | 
| CHIP | Chip errata workarounds initialization API | 
| CMU | Clock management unit (CMU) Peripheral API | 
| COMMON | General purpose utilities and cross-compiler support | 
| CORE | Core interrupt handling API | 
| CRYOTIMER | Ultra Low Energy Timer/Counter (CRYOTIMER) Peripheral API | 
| CRYPTO | Cryptography accelerator peripheral API | 
| CSEN | Capacitive Sense (CSEN) Peripheral API | 
| DBG | Debug (DBG) Peripheral API | 
| EMU | Energy Management Unit (EMU) Peripheral API | 
| GPCRC | General Purpose Cyclic Redundancy Check (GPCRC) API | 
| GPIO | General Purpose Input/Output (GPIO) API | 
| I2C | Inter-integrated Circuit (I2C) Peripheral API | 
| IDAC | Current Digital-to-Analog Converter (IDAC) Peripheral API | 
| INT | Safe nesting of interrupt disable/enable API | 
| LDMA | Linked Direct Memory Access (LDMA) Peripheral API | 
| LESENSE | Low Energy Sensor (LESENSE) Peripheral API | 
| LETIMER | Low Energy Timer (LETIMER) Peripheral API | 
| LEUART | Low Energy Universal Asynchronous Receiver/Transmitter (LEUART) Peripheral API | 
| MPU | Memory Protection Unit (MPU) Peripheral API | 
| MSC | Memory System Controller API | 
| OPAMP | Operational Amplifier (OPAMP) peripheral API | 
| PCNT | Pulse Counter (PCNT) Peripheral API | 
| PRS | Peripheral Reflex System (PRS) Peripheral API | 
| RAMFUNC | RAM code support | 
| RMU | Reset Management Unit (RMU) Peripheral API | 
| RTCC | Real Time Counter (RTCC) Peripheral API | 
| SMU | Security Management Unit (SMU) Peripheral API | 
| SYSTEM | System API | 
| TIMER | Timer/Counter (TIMER) Peripheral API | 
| USART | Universal Synchronous/Asynchronous Receiver/Transmitter Peripheral API | 
| VDAC | Digital to Analog Voltage Converter (VDAC) Peripheral API | 
| VERSION | Version API | 
| WDOG | Watchdog (WDOG) Peripheral API | 
| External Device Drivers | External Device Drivers is a collection of device drivers for external components. These components are typically Silicon Laboratories ICs that are not part of the Gecko families of SoCs | 
| EFP Driver | EFP (Energy Friendly PMIC) driver | 
| Kit Drivers | Kit support and drivers | 
| CPT112S_I2C | Silicon Labs 12-pad Capacitive Touch Evaluation Board I2C driver | 
| CapSense | Capacitive sensing driver | 
| Display | Display device driver stack library | 
| DmaCtrl | UDMA control block array | 
| EEPROM | I2C EEPROM Driver | 
| Gecko USB MSD | USB Mass Storage Class (MSC) | 
| Gecko USB RS232 bridge | Gecko USB to RS232 bridge (CDC Class) | 
| HidKeyboard | Implements a USB HID class keyboard | 
| I2CSPM | I2C Simple Polled Master driver | 
| Ksz8851snl | KSZ8851SNL SPI Ethernet Controller driver | 
| MicroSd | SPI driver for micro SD card | 
| NANDFlash | Driver for Numonyx NAND256W3A NAND Flash devices | 
| NORFlash | Driver for Spanion S29GL128P90FFIR13 and S29GL064N NOR Flash devices | 
| RetargetIo | Standard I/O retargeting driver | 
| SegmentLcd | Segment LCD driver | 
| Si114x | Silicon Labs Si114x Ultraviolet (UV) Index, Gesture, Proximity, and Ambient Light Sensor I2C driver | 
| Si7013 | Silicon Labs Si7013 Relative Humidity and Temperature Sensor I2C driver | 
| Si72xx | Silicon Labs Si72xx Magnetic Hall Effect Sensor I2C driver | 
| TFT | Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode | 
| TempSensor | Driver for DS75 I2C temperature sensor | 
| Textdisplay | Line based text output terminal interface on top of the DISPLAY device driver stack. See TextDisplay Library for more information | 
| Touch | Touch panel driver for DK3650, DK3750 and DK3850 Development Kits | 
| Udelay | Calibrated busy wait loop | 
| UsbHid | USB HID keyboard scan codes | 
| VddCheck | VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API | 
| Platform Common | Gecko Platform Common components are used throughout the Gecko SDK | 
| BIT | |
| SLIST | |
| Status Codes | |
| Platform Middleware | Gecko Platform Middleware for use with EFM32, EZR32 and EFR32 products | 
| Capacitive Sensing Firmware Library | Capacitive sensing firmware library for Silicon Labs MCUs | 
| GLIB | Graphics Library | 
| Platform Services | Gecko Platform Service components are high-level, device-independent and thread-safe APIs. Each service may have a hardware abstraction layer (HAL) | 
| MPU | MPU basic utilities | 
| SLEEPTIMER | Low frequency timer utilities. Utilities (timer, delays and time keeping) |