LDMA initialization configuration structure.
       Definition at line
       
        877
       
       of file
       
        em_ldma.h
       
       .
      
      
       #include <
       
     
        em_ldma.h
       
       >
      
| Data Fields | |
| uint8_t | ldmaInitCtrlNumFixed | 
| uint8_t | ldmaInitCtrlSyncPrsClrEn | 
| uint8_t | ldmaInitCtrlSyncPrsSetEn | 
| uint8_t | ldmaInitIrqPriority | 
Field Documentation
| uint8_t LDMA_Init_t::ldmaInitCtrlNumFixed | 
Arbitration mode separator.
        Definition at line
        
         878
        
        of file
        
         em_ldma.h
        
        .
       
Referenced by DMADRV_Init() , and LDMA_Init() .
| uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsClrEn | 
| uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsSetEn | 
| uint8_t LDMA_Init_t::ldmaInitIrqPriority | 
LDMA IRQ priority (0..7).
        Definition at line
        
         881
        
        of file
        
         em_ldma.h
        
        .
       
Referenced by DMADRV_Init() , and LDMA_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_ldma.h