ARRAY_TypeDef Struct Reference
Defines segment COM and BIT fields for array.
       Definition at line
       
        136
       
       of file
       
        segmentlcd.c
       
       .
      
| Data Fields | |
| uint8_t | bit [35] | 
| uint8_t | com [35] | 
Field Documentation
| uint8_t ARRAY_TypeDef::bit[35] | 
LCD bit number
        Definition at line
        
         138
        
        of file
        
         segmentlcd.c
        
        .
       
| uint8_t ARRAY_TypeDef::com[35] | 
LCD COM line (for multiplexing)
        Definition at line
        
         137
        
        of file
        
         segmentlcd.c
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/hardware/kit/common/drivers/
       segmentlcd.c