TIMER initialization structure.
       Definition at line
       
        269
       
       of file
       
        em_timer.h
       
       .
      
      
       #include <
       
     
        em_timer.h
       
       >
      
| Data Fields | |
| bool | ati | 
| TIMER_ClkSel_TypeDef | clkSel | 
| bool | count2x | 
| bool | debugRun | 
| bool | dmaClrAct | 
| bool | enable | 
| TIMER_InputAction_TypeDef | fallAction | 
| TIMER_Mode_TypeDef | mode | 
| bool | oneShot | 
| TIMER_Prescale_TypeDef | prescale | 
| bool | quadModeX4 | 
| TIMER_InputAction_TypeDef | riseAction | 
| bool | sync | 
Field Documentation
| bool TIMER_Init_TypeDef::ati | 
ATI (Always Track Inputs) makes CCPOL always track the polarity of the inputs.
        Definition at line
        
         288
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| TIMER_ClkSel_TypeDef TIMER_Init_TypeDef::clkSel | 
| bool TIMER_Init_TypeDef::count2x | 
2x Count mode, counter increments/decrements by 2, meant for PWM mode.
        Definition at line
        
         284
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| bool TIMER_Init_TypeDef::debugRun | 
Counter shall keep running during debug halt.
        Definition at line
        
         274
        
        of file
        
         em_timer.h
        
        .
       
Referenced by BOARD_init() , and TIMER_Init() .
| bool TIMER_Init_TypeDef::dmaClrAct | 
DMA request clear on active.
        Definition at line
        
         301
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| bool TIMER_Init_TypeDef::enable | 
Start counting when initialization completed.
        Definition at line
        
         271
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| TIMER_InputAction_TypeDef TIMER_Init_TypeDef::fallAction | 
Action on falling input edge.
        Definition at line
        
         292
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| TIMER_Mode_TypeDef TIMER_Init_TypeDef::mode | 
| bool TIMER_Init_TypeDef::oneShot | 
Determines if only counting up or down once.
        Definition at line
        
         307
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| TIMER_Prescale_TypeDef TIMER_Init_TypeDef::prescale | 
Prescaling factor, if HFPER / HFPERB clock used.
        Definition at line
        
         277
        
        of file
        
         em_timer.h
        
        .
       
Referenced by BOARD_init() , TIMER_Init() , and USTIMER_Init() .
| bool TIMER_Init_TypeDef::quadModeX4 | 
Select X2 or X4 quadrature decode mode (if used).
        Definition at line
        
         304
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| TIMER_InputAction_TypeDef TIMER_Init_TypeDef::riseAction | 
Action on rising input edge.
        Definition at line
        
         295
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
| bool TIMER_Init_TypeDef::sync | 
Timer start/stop/reload by other timers.
        Definition at line
        
         310
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_timer.h