EUSART_IrDAInit_TypeDef Struct Reference
IrDA Initialization structure.
Definition at line
259
of file
em_eusart.h
.
#include <
em_eusart.h
>
Data Fields |
|
| EUSART_UartInit_TypeDef | init |
|
General EUSART initialization structure.
|
|
| bool | irDALowFrequencyEnable |
|
Enable the IrDA low frequency mode. Only Rx operation are enabled.
|
|
EUSART_IrDAPulseWidth_Typedef
|
irDAPulseWidth |
EUSART_IrDARxFilterEnable_TypeDef
|
irDARxFilterEnable |
|
Set to enable filter on IrDA demodulator.
|
|
Field Documentation
EUSART_IrDAPulseWidth_Typedef
EUSART_IrDAInit_TypeDef::irDAPulseWidth
|
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
Definition at line
271
of file
em_eusart.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super/platform/emlib/inc/
em_eusart.h