MIC - Microphone Driver (ADC)
Detailed Description
Driver for the Knowles SPV1840LR5H-B MEMS Microphone.
Functions | |
void | MIC_deInit (void) |
Powers down the MEMS microphone stops the ADC and frees up the DMA channel. | |
float | MIC_getMean (void) |
Calculates the average value of the samples in the buffer. | |
uint16_t * | MIC_getSampleBuffer (void) |
Gets the sample buffer. | |
float | MIC_getSoundLevel (float *var) |
Calculates the sound level. | |
uint32_t | MIC_init (uint32_t fs, uint16_t *buffer, size_t len) |
Initializes MEMS microphone and sets up the DMA, ADC and clocking. | |
bool | MIC_isBusy (void) |
Checks if the microphone is in use. | |
void | MIC_start (uint32_t nSamples) |
Starts taking samples using DMA from the microphone. | |
Error Codes | |
#define | MIC_OK 0 |
Macro Definition Documentation
#define MIC_OK 0 |
No errors
Definition at line 58
of file mic.h
.
Function Documentation
void MIC_deInit | ( | void |
| ) |
Powers down the MEMS microphone stops the ADC and frees up the DMA channel.
- Returns
- None
Definition at line 189
of file mic.c
.
References BOARD_micEnable(), DMADRV_FreeChannel(), and PRS_SourceAsyncSignalSet().
float MIC_getMean | ( | void |
| ) |
Calculates the average value of the samples in the buffer.
- Returns
- The mean value of the samples in the buffer
Definition at line 262
of file mic.c
.
Referenced by MIC_getSoundLevel().
uint16_t * MIC_getSampleBuffer | ( | void |
| ) |
Gets the sample buffer.
- Returns
- Returns a pointer to the sample buffer
Definition at line 250
of file mic.c
.
float MIC_getSoundLevel | ( | float * | var | ) |
Calculates the sound level.
- Parameters
-
[out] var
The variance of the samples
- Returns
- The sound level in dB
Definition at line 287
of file mic.c
.
References MIC_getMean().
uint32_t MIC_init | ( | uint32_t | fs, |
uint16_t * | buffer, |
||
size_t | len |
||
) |
Initializes MEMS microphone and sets up the DMA, ADC and clocking.
- Parameters
-
[in] fs
The desired sample rate in Hz [in] buffer
Pointer to the sample buffer to store the ADC data [in] len
The size of the sample buffer
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 93
of file mic.c
.
References ADC_Init(), ADC_INIT_DEFAULT, ADC_InitScan(), ADC_INITSCAN_DEFAULT, ADC_PrescaleCalc(), ADC_ScanInputClear(), ADC_ScanSingleEndedInputAdd(), ADC_TimebaseCalc(), adcInit(), adcRef2V5, BOARD_micEnable(), CMU_ClockEnable(), CMU_ClockFreqGet(), CMU_ClockSelectSet(), cmuClock_ADC0, cmuClock_AUX, cmuClock_LFA, cmuClock_PRS, cmuSelect_LFXO, LETIMER_Init_TypeDef::comp0Top, DMADRV_AllocateChannel(), DMADRV_Init(), ECODE_EMDRV_DMADRV_OK, ADC_Init_TypeDef::em2ClockConfig, LETIMER_Init_TypeDef::enable, LETIMER_CompareSet(), LETIMER_Init(), LETIMER_INIT_DEFAULT, LETIMER_RepeatSet(), letimerUFOAPulse, ADC_Init_TypeDef::prescale, PRS_SourceAsyncSignalSet(), ADC_InitScan_TypeDef::prsEnable, ADC_InitScan_TypeDef::prsSel, ADC_InitScan_TypeDef::reference, ADC_InitScan_TypeDef::scanDmaEm2Wu, ADC_Init_TypeDef::timebase, and LETIMER_Init_TypeDef::ufoa0.
bool MIC_isBusy | ( | void |
| ) |
Checks if the microphone is in use.
- Returns
- Returns true if the DMA is busy taking microphone samples
Definition at line 326
of file mic.c
.
void MIC_start | ( | uint32_t | nSamples | ) |
Starts taking samples using DMA from the microphone.
- Parameters
-
[in] nSamples
The number of the samples to take
- Returns
- None
Definition at line 215
of file mic.c
.
References DMADRV_PeripheralMemory(), dmadrvDataSize2, and dmadrvPeripheralSignal_ADC0_SCAN.