EZRADIODRV_AutoAckHandle Struct Reference
EzRadio auto acknowledge plug-in instance initialization and handler structure.
Definition at line 76
of file ezradio_auto_ack_plugin.h
.
#include <
ezradio_auto_ack_plugin.h
>
Data Fields | |
EZRADIODRV_AutoAckMode_t | ackMode |
Auto ack mode. | |
EZRADIODRV_PacketLengthConfig_t | lenConfig |
Pakcet length config for auto ack. | |
uint8_t * | pktBuf |
Pointer to the buffer that holds the auto ack packet. | |
uint16_t | pktId |
Auto ack packet ID. | |
EZRADIODRV_AutoAckPacketMode_t | pktMode |
Packet mode for aut ack. | |
EZRADIODRV_Callback_t | userCallback |
User callback. | |
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emdrv/ezradiodrv/plugins/inc/
ezradio_auto_ack_plugin.h