__BMP_DataType Struct Reference
BMP Data type structure to hold information about the bmp data returned.
Definition at line 142
of file bmp.h
.
#include <
bmp.h
>
Data Fields | |
uint16_t | bitsPerPixel |
uint32_t | compressionType |
uint32_t | endOfRow |
uint32_t | size |
Field Documentation
uint16_t __BMP_DataType::bitsPerPixel |
Color depth of the data returned from function.
Definition at line 144
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), and BMP_readRawDataRLE8().
uint32_t __BMP_DataType::compressionType |
Compression type
Definition at line 146
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), and BMP_readRawDataRLE8().
uint32_t __BMP_DataType::endOfRow |
Marks whether this data is at the end of the current row. endOfRow == 1, if end of row is reached. endOfRow == 0, if there is still unread data left in the row
Definition at line 150
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRawDataRLE8(), BMP_readRgbData(), BMP_readRgbDataRLE8(), and BMP_readRleData().
uint32_t __BMP_DataType::size |
Byte length of returned data
Definition at line 148
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRawDataRLE8(), and BMP_readRgbData().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/middleware/glib/glib/
bmp.h