__GLIB_Context_t Struct Reference

GLIB Drawing Context (Multiple instances of GLIB_Context_t can exist)

Definition at line 270 of file glib.h .

#include < glib.h >

Data Fields

uint32_t backgroundColor
GLIB_Rectangle_t clippingRegion
GLIB_Font_t font
uint32_t foregroundColor
const DMD_DisplayGeometry * pDisplayGeometry

Field Documentation

uint32_t __GLIB_Context_t::backgroundColor

Background color

Definition at line 275 of file glib.h .

Referenced by GLIB_clear() , GLIB_clearRegion() , GLIB_contextInit() , and GLIB_drawChar() .

GLIB_Font_t __GLIB_Context_t::font

Font definition

Definition at line 284 of file glib.h .

Referenced by GLIB_drawChar() , GLIB_drawString() , and GLIB_setFont() .

uint32_t __GLIB_Context_t::foregroundColor

Foreground color

Definition at line 278 of file glib.h .

Referenced by GLIB_contextInit() , GLIB_drawLineH() , GLIB_drawLineV() , GLIB_drawPixel() , and GLIB_drawRectFilled() .

const DMD_DisplayGeometry* __GLIB_Context_t::pDisplayGeometry

Pointer to the dimensions of the display

Definition at line 272 of file glib.h .

Referenced by GLIB_clear() , GLIB_contextInit() , GLIB_resetClippingRegion() , GLIB_resetDisplayClippingArea() , and GLIB_setClippingRegion() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/middleware/glib/glib/ glib.h