COMMON
Detailed Description
General purpose utilities and cross-compiler support.
This SDK supports the following compilers/IDEs:
- Simplicity Studio
- IAR Embedded Workbench
- Keil µVision IDE
- Plain armgcc
Certain compiler features such as alignment is implemented differently in the tools. Therefore, macros such as SL_ALIGN are provided to enable compiler independent code.
- Note
- RAM code macros are implemented in a separate module RAMFUNC . Cross-compiler RAM code support needs extended documentation and it is therefore implemented as a separate module.
Macros |
|
| #define | SL_ALIGN (X) |
|
A macro for aligning a variable.
Use this macro before the variable definition. X denotes the storage alignment value in bytes. To be GCC-compatible, use SL_ATTRIBUTE_ALIGN(X) before the semicolon on normal variables. Use SL_ATTRIBUTE_ALIGN(X) before the opening curly brace on structure variables. |
|
| #define | SL_ATTRIBUTE_ALIGN (X) __attribute__ ((aligned(X))) |
|
GCC style macro for aligning a variable.
|
|
| #define | SL_ATTRIBUTE_PACKED __attribute__ ((packed)) |
|
A GCC style macro for handling packed structures.
|
|
| #define | SL_ATTRIBUTE_SECTION (X) __attribute__ ((section(X))) |
| #define | SL_CEILING (n, i) ((((n) + (i) - 1U) / (i)) * (i)) |
|
Round n up to closest interval of i.
|
|
| #define | SL_FALLTHROUGH |
|
A macro for notifying the compiler of an intended switch case fallthrough.
|
|
| #define | SL_FLOOR (n, i) ((n / i) * i)) |
|
Round n down to closest interval of i.
|
|
| #define | SL_MAX (a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a > _b ? _a : _b; }) |
|
A macro for getting the maximum value. No sideeffects, a and b are evaluated one time only.
|
|
| #define | SL_MIN (a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a < _b ? _a : _b; }) |
|
A macro for getting the minimum value. No sideeffects, a and b are evaluated one time only.
|
|
| #define | SL_NORETURN __attribute__ ((noreturn)) |
|
A macro for handling non-returning functions.
|
|
| #define | SL_PACK_END () |
|
A macro for handling packed structures.
Use this macro after the structure definition. With GCC, add SL_ATTRIBUTE_PACKED after the closing curly braces of the structure definition. |
|
| #define | SL_PACK_START (x) |
|
A macro for handling packed structures.
Use this macro before the structure definition. X denotes the maximum alignment of structure members. X is not supported with GCC. GCC always uses 1 byte maximum alignment. |
|
| #define | SL_WEAK __attribute__ ((weak)) |
|
A macro for defining a weak symbol.
|
|
| #define | STRINGIZE (X) #X |
|
Stringify X.
|
|
Functions |
|
| __STATIC_INLINE uint32_t | EFM32_CTZ (uint32_t value) |
| __STATIC_INLINE uint32_t | SL_CTZ (uint32_t value) |
|
Count trailing number of zeros. Use CLZ instruction if available.
|
|
| __STATIC_INLINE uint32_t | SL_Log2ToDiv (uint32_t log2) |
|
Convert logarithm of 2 to division factor.
|
|
| __STATIC_INLINE uint32_t | SL_RBIT (uint32_t value) |
|
Reverse the bits. Use the RBIT instruction if available, else process.
|
|
| __STATIC_INLINE uint32_t | SL_RBIT16 (uint32_t value) |
|
Reverse the bits. Use the RBIT instruction if available, else process.
|
|
Macro Definition Documentation
| #define SL_ATTRIBUTE_SECTION | ( |
X
|
) | __attribute__ ((section(X))) |
A macro for placing a variable in a section.
Use this macro after the variable definition, before the equal sign or a semicolon.
X denotes the section to place the variable in.
Definition at line
200
of file
em_common.h
.
Function Documentation
| __STATIC_INLINE uint32_t SL_CTZ | ( | uint32_t |
value
|
) |
Count trailing number of zeros. Use CLZ instruction if available.
- Parameters
-
[in] valueData value to check for number of trailing zero bits.
- Returns
- A number of trailing zeros in value.
Definition at line
222
of file
em_common.h
.
Referenced by GPIOINT_CallbackRegister() .
| __STATIC_INLINE uint32_t SL_Log2ToDiv | ( | uint32_t |
log2
|
) |
Convert logarithm of 2 to division factor.
- Parameters
-
[in] log2Logarithm of 2.
- Returns
- Dividend.
Definition at line
297
of file
em_common.h
.
| __STATIC_INLINE uint32_t SL_RBIT | ( | uint32_t |
value
|
) |
Reverse the bits. Use the RBIT instruction if available, else process.
- Parameters
-
[in] valueData value to reverse.
- Returns
- A reversed value.
Definition at line
252
of file
em_common.h
.
Referenced by SL_RBIT16() .
| __STATIC_INLINE uint32_t SL_RBIT16 | ( | uint32_t |
value
|
) |
Reverse the bits. Use the RBIT instruction if available, else process.
- Parameters
-
[in] value16-bit data value to reverse.
- Returns
- A 16-bit reversed value.
Definition at line
282
of file
em_common.h
.
References SL_RBIT() .