MSDSCSI_Inquiry_TypeDef Struct Reference
SCSI Inquiry Command Descriptor Block (CDB) typedef.
       Definition at line
       
        71
       
       of file
       
        msdscsi.h
       
       .
      
      
       #include <
       
     
        msdscsi.h
       
       >
      
         Data Fields | 
       |
| struct { | |
| uint8_t Evpd : 1 | |
| uint8_t Obsolete : 1 | |
| uint8_t Reserved : 6 | |
| }; | |
| uint16_t | AllocationLength | 
| uint8_t | Control | 
| uint8_t | OpCode | 
| uint8_t | PageCode | 
Field Documentation
| uint16_t MSDSCSI_Inquiry_TypeDef::AllocationLength | 
Number of inquiry data bytes requested.
        Definition at line
        
         79
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_Inquiry_TypeDef::Control | 
Control byte.
        Definition at line
        
         80
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_Inquiry_TypeDef::Evpd | 
Enable Vital Product data.
        Definition at line
        
         74
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_Inquiry_TypeDef::Obsolete | 
Obsolete, expect any value.
        Definition at line
        
         75
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_Inquiry_TypeDef::OpCode | 
Command opcode.
        Definition at line
        
         72
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_Inquiry_TypeDef::PageCode | 
Pagecode.
        Definition at line
        
         78
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_Inquiry_TypeDef::Reserved | 
Reserved, expect 0.
        Definition at line
        
         76
        
        of file
        
         msdscsi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/hardware/kit/common/drivers/
       
msdscsi.h